你好:
产品中有用到TMS320C6748+TMS320C6746两颗DSP,双核通信,采用SPI直接连接,同时增加两个IO口直连(中间有串联1K电阻),用来提高SPI双核通信效率,待机状态下,SPI总线时钟会关闭,通过IO口电平翻转,激活SPI接口,目前遇到的问题是,IO口概率性无法按照软件输出高低电平(概率比较低,无法拉高或者拉低),导致双核通信异常,帮忙分析一下如下硬件连接是否存在问题及该问题可能产生的原因.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
产品中有用到TMS320C6748+TMS320C6746两颗DSP,双核通信,采用SPI直接连接,同时增加两个IO口直连(中间有串联1K电阻),用来提高SPI双核通信效率,待机状态下,SPI总线时钟会关闭,通过IO口电平翻转,激活SPI接口,目前遇到的问题是,IO口概率性无法按照软件输出高低电平(概率比较低,无法拉高或者拉低),导致双核通信异常,帮忙分析一下如下硬件连接是否存在问题及该问题可能产生的原因.
补充两个现象:
1. DSPC6748 GP8[12] GPIO设置为输入状态,内部和外部没有上下拉,常温下测试是高电平3.3V,高位60℃变为低电平0V,是否正常?
2. DSPC6748 GP6[13] 设置输出0V,连接DSPC6746 GP8[2]设置输入3.3V, 常温下连接之后是0V, 高温60℃连接后是3.3V, 不知是何原因?