当前所用的6614 Linux kernel的版本,Nand驱动Davinci_nand.c不支持4KB-page的Nand,只支持到2KB,请问哪里可能下载到最新的6614 Kernel版本?
static int __init nand_davinci_probe(struct platform_device *pdev)
{
/* 4KiB page chips are not yet supported. The eccpos from
* nand_ecclayout cannot hold 80 bytes and change to eccpos[]
* breaks userspace ioctl interface with mtd-utils. Once we
* resolve this issue, NAND_ECC_HW_OOB_FIRST mode can be used
* for the 4KiB page chips.
*
* TODO: Note that nand_ecclayout has now been expanded and can
* hold plenty of OOB entries.
*/
}