最近在调试NOR Flash,C6657的EMIF地址线只有24根,但是CE1连接的NOR Flash有27根地址线,现在用3个GPIO作为flash的高地址扩展,请问用GPIO做高地址扩展时程序上应该怎么编写,现在完全没有思路,恳请大神指导
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在调试NOR Flash,C6657的EMIF地址线只有24根,但是CE1连接的NOR Flash有27根地址线,现在用3个GPIO作为flash的高地址扩展,请问用GPIO做高地址扩展时程序上应该怎么编写,现在完全没有思路,恳请大神指导
可以这样理解GPIO做高地址时的地址范围
GPIO2GPIO2GPIO0A23A22.....A1A0:
00000......00
00000......01
.................... 16M
00011......11
00100.......00
00100.......01
..................... 16M
00111........11
..................... .....
.....................
11100.........00
11100..........01
...................... 16M
11111..........11