My K2G EVM development board failed to start through EMMC.
Operation steps:
1. After using SD card, EMMC is divided into FAT32 and ext3;
2. Compile the U boot with the default configuration of K2G ﹣ EVM ﹣ defconfig, and copy the MLO and u-boot.img files to the FAT32 partition
3. Turn the dial switch to EMMC start and turn on the power.
What are the wrong operations? What should I do to successfully start from EMMC? I hope to get some help. Thank you very much.
我的K2G evm开发板,通过emmc启动不成功。
操作步骤:
1、使用SD卡启动后,将emmc分区,分为Fat32和ext3格式的两个区;
2、使用k2g_evm_defconfig默认配置编译Uboot,将MLO和u-boot.img文件拷贝到Fat32分区
3、将拨码开关调到EMMC启动,接通电源。
哪些操作是错误的,我应该怎样做才能成功从EMMC启动,希望得到一些帮助,非常感谢。