您好,将K1_STK_v1.1中GE例程按照论坛中的方式修改为UDP发包,使用Wireshark在PC端抓包发现数据丢包较频繁,现有以下问题想咨询下:
1,PC端丢包可能的原因是什么?
2,程序GE_2DSP_Test.c文件中有注释如下
/*Fllowing table specifies the packet transfered on 2 ports,
number of packets of each port should be less than 64 for this test*/
注释中提到的numPackets要少于64包是由于什么被限制了?以及payloadNumBytes参数是否有大小限制?
3,GE_2DSP_Test函数中有如下语句
//delay to avoid potentail overflow, for debug only
TSC_delay_ms(DELAY_BETWEEN_PACKET_MS);
注释中提到的调试模式下放开该语句,想咨询下正式程序中是否有加该语句的必要?