This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WIN10操作系统如何配置CCS的环境变量

看了文档PRU ICSS EtherCAT Slave User Guide,里面提到要设置CCS的环境变量,我搜了些资料,配置了在WIN10环境下的环境变量,然后在命令行里根据文档的步骤执行以下命令行

  • Open Command/Shell Prompt and navigate to [INSTALL-DIR]/protocols/<protocol name>/projects
  • Run projectCreate.bat or projectCreate.sh. The batch file takes three mandatory command line arguments (The mandatory arguments are case sensitive!)

Usage format: projectCreate.bat [SOC] [PROCESSOR] [PROJECT_NAME]

  • [SOC]
    • The valid values for first command line argument [SOC] are
      • AM571x - To generate a project specific to AM571x
      • AM572x - To generate a project specific to AM572x
      • AM437x - To generate a project specific to AM437x
      • AM335x - To generate a project specific to AM335x
      • AMIC11x - To generate a project specific to AMIC11x
      • AMIC12x - To generate a project specific to AMIC12x
      • K2G - To generate a project specific to K2G
      • AM65xx - To generate a project specific to AM65xx
  • [PROCESSOR]
    • The valid values for second command line argument [PROCESSOR] are
      • arm - To generate a project specific to ARM core
  • [PROJECT_NAME]
    • The valid values for third command line argument [PROJECT_NAME] to be used with EtherCAT slave installer package
      • ethercat_slave_full - to generate EtherCAT slave full application project
      • ethercat_slave_demo - to generate EtherCAT slave demo application project
      • ecat_ti_esc_spi_master - to generate EtherCAT TI ESC SPI Mode Master application project (supported only for AM572x)
      • ecat_ti_esc_spi_slave - to generate EtherCAT TI ESC SPI Mode Slave (ASIC Mode) application project (supported only for AMIC11x)
      • ethercat_slave_cia402 - to generate Single-Chip Motor-Control application through Standard CiA402 Drive Profile over EtherCAT (supported only for AM437x)

我的板子是K2GICE,配置完毕,命令行显示的是路径错误,尝试了很多次,依然失败

Note