由于国庆节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解。

C6678的0核LOAD程序失败

板卡是自己设计的,用的仿真器是合众达的XDS560 PLUS,TCK设置为了500KHz,连上之后,load程序,大小1.3M。

CCS5.4显示错误:

C66xx_0: Trouble Reading Register ControlRegisters_CSR: (Error -1060 @ 0x41) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)

C66xx_0: Trouble Reading Register ControlRegisters_CSR: (Error -1060 @ 0x41) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)

C66xx_0: Trouble Writing Memory Block at 0xc07ffd0 on Page 0 of Length 0x36f7: (Error -1060 @ 0x64) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)

C66xx_0: GEL: File: D:\zougj\project\test\C6678_GE_testRecv.out: Load failed.

C66xx_0: Trouble Reading Register ControlRegisters_CSR: (Error -1060 @ 0x41) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)

如图中,0核连上后会出现“No source available for "0x70186bd8""这个问题。

但是用其他几个核load就没有出现load failed问题。

请专家们给出建议。