我司采用主控DM8107,DDR3采用MT41K128M16JT-125:K,启动过程中会出现随机事件导致系统无法运行(串口,看门狗等均无法作用,只能强制断电或复位),后经测试随机事件中,发现DDR3未进行复位,DM385没有送出DDR复位信号,uboot没有进入第二阶段
已排查:1.电源电压正常且电流无异常2.电源上电顺序正常,3.一旦启动系统启动运行稳定
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
十分感谢你的建议,因为目前我们无法进行SW leveling,我们又做了大量测试以便于让问题更加清晰。
通过大量测试,
我们发现,DDR复位信号(引脚端号:AA20 DDR[0]_RSTN)正常启动时DDR复位信号会产生一个复位脉冲,异常启动无法开机时一定不会产生该脉冲
1.在启动过程中,是否存在事件导致DDR复位异常
2.DDR正常复位前,已经完成那些工作,要进行那些工作