This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138上电启动不成功问题,困扰好久

Other Parts Discussed in Thread: OMAP-L138

目前设计的OMAPL138上电启动遇到问题比较奇怪,希望能给解答下:

现象,

一、上电问题

1、OMAPL138初次上电启动不成功,紧接着第二次上电能给正常启动;

2、OMAPL138再次下电,等一分钟左右时间,又会出现上电不成功现象,但是在短时间内进行再次上电能给正常启动

二、上电电源1.8V变2.4V问题

1、采用线性直流电源供电,用滑行开关控制上下电,上电后捕捉1.8V电源电压,发现电源电压在2.4V左右;

2、采用开关电源或其他类型电源没有出现过该现象,仅仅在使用线性直流电源供电时发现过

三、目前的设计

复位电路采用CAT809复位芯片,上电时序先后正确核电压、1.8V、最后3.3V