The maximum resolution for the LCD controller is 2048 × 2048 pixels. The maximum frame rate is
determined by the image size in combination with the pixel clock rate.
请问AM3358的图像处理的最小分辨率和最高帧率是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AM335x LCDC的时钟频率可以达到126MHz.
http://processors.wiki.ti.com/index.php/AM335x_LCD_Controller_Driver's_Guide
#2. 按照帧频计算方法。帧频=126.5MHz/(1920x1080x1.3)约为47MHz。
max frame rate = PCLK / (X * Y * 1.3)