This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 ddr和flash支援問題

Other Parts Discussed in Thread: AM3352

Hi

請問AM3352 ddr和flash最大可以支援的容量是多少?我在datasheet沒看到資料

謝謝

Daniel

  • EMIF 支持 1GB 全部可寻址空间
    • 外部存储器接口 (EMIF)
    – mDDR(LPDDR)、DDR2、DDR3、DDR3L 控制
    器:
    – mDDR:200MHz 时钟(400MHz 数据速率)
    – DDR2:266MHz 时钟(532MHz 数据速率)
    – DDR3:400MHz 时钟(800MHz 数据速率)
    – DDR3L:400MHz 时钟rug(800MHz 数据速率)
    – 16 位数据总线
    – 1GB 全部可寻址空间
    – 支持一个 x16 或两个 x8 存储器件配置
    GPMC最大可寻址512MB
    which can be divSupport 512M Bytes maximum addressing capabilityided into seven independent
    chip-select with programmable bank size and base address on 16M Bytes, 32M Bytes, 64M Bytes, or
    128M Bytes boundary
    另外 nand flash不是通过GPMC地址线寻址,大小不受限制。