This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问AM3359的电平驱动电流问题

Other Parts Discussed in Thread: AM3359, MAX3232, MAX232

AM3359芯片UART_RXD的电流参数如图,请问正常3.3v工作状态下驱动UART_RXD变成高电平和低电平所需要的电流,是18uA还是其他值呢,多谢!

MAX3232数据手册里面的ROUT输出高电平时最多可以输出1mA,请问MAX3232的一个ROUT管脚最多可以驱动多少个AM3359的UART_RXD管脚,多谢!

  • 您好,

    您是打算一个UART口下连接多个UART吗,我认为UART不属于总线通信,不能同时接2个或2个以上通信。
    18uA应该指的是Receiver disabled、pullup or pulldown禁止时的输入漏电流。即使MAX3232的一个ROUT管脚可以实现驱动多路,也有PCB的设计有关,因为PCB信号线会产生寄生电容,驱动寄生电容也需要电流。
  • 是的,UART是点对点双向通信,我们现在只需要单向的一路MAX232芯片数据传给2个AM3359,2个AM3359只收不发,所以才询问驱动电流问题,如果不用这种直连方式,TI是否有类似的逻辑电平驱动芯片,即一路TTL输入转成多个同样的TTL输出,多谢!