大家好,我将am335x-evm板的flash改为(–Page size x8: 4320 bytes (4096 + 224 bytes)),请问uboot需要修改那些地方?
我之前修改了am335x_evm.h后。
在uboot显示如下结果
=> mtdpart
default nand0: partition (NAND.SPL) size alignment incorrect
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我将am335x-evm板的flash改为(–Page size x8: 4320 bytes (4096 + 224 bytes)),请问uboot需要修改那些地方?
我之前修改了am335x_evm.h后。
在uboot显示如下结果
=> mtdpart
default nand0: partition (NAND.SPL) size alignment incorrect
你好,请问am335x_evm.h文件中mtdparts配置是指哪里?
我查看了文件仅有:
#ifdef CONFIG_NAND
#define NANDARGS \
"mtdids=" CONFIG_MTDIDS_DEFAULT "\0" \
"mtdparts=" CONFIG_MTDPARTS_DEFAULT "\0" \
"nandargs=setenv bootargs console=${console} " \
"${optargs} " \
"root=${nandroot} " \
"rootfstype=${nandrootfstype}\0" \
"nandroot=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048\0" \
"nandrootfstype=ubifs rootwait=1\0" \
"nandboot=echo Booting from nand ...; " \
"run nandargs; " \
"nand read ${fdtaddr} NAND.u-boot-spl-os; " \
"nand read ${loadaddr} NAND.kernel; " \
"bootz ${loadaddr} - ${fdtaddr}\0"
#else
#define NANDARGS ""
#endif
这一处提到了mdtparts,里面涉及的CONFIG_MTDPARTS_DEFAULT 在am335x_evm_deconfig中出现:
CONFIG_MTDPARTS_DEFAULT="mtdparts=nand.0:128k(NAND.SPL),128k(NAND.SPL.backup1),128k(NAND.SPL.backup2),128k(NAND.SPL.backup3),256k(NAND.u-boot-spl-os),1m(NAND.u-boot),128k(NAND.u-boot-env),128k(NAND.u-boot-env.backup1),8m(NAND.kernel),-(NAND.file-system)"
这里面有需要修改的参数?另外附上我之前修改的am335x_evm.h的部分:
#ifdef CONFIG_NAND
/* NAND: device related configs */
#define CONFIG_SYS_NAND_5_ADDR_CYCLE
#define CONFIG_SYS_NAND_PAGE_COUNT (CONFIG_SYS_NAND_BLOCK_SIZE / \
CONFIG_SYS_NAND_PAGE_SIZE)
#define CONFIG_SYS_NAND_PAGE_SIZE 4096
#define CONFIG_SYS_NAND_OOBSIZE 224/*64*/
#define CONFIG_SYS_NAND_BLOCK_SIZE (128*2048)/*128*1024*/
/* NAND: driver related configs */
#define CONFIG_SYS_NAND_BAD_BLOCK_POS NAND_LARGE_BADBLOCK_POS
#define CONFIG_SYS_NAND_ECCPOS { 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, \
16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, \
28, 29, 30, 31, 32, 33, 34, 35, 36, 37, 38, 39, \
40, 41, 42, 43, 44, 45, 46, 47, 48, 49, 50, 51, \
52, 53, 54, 55, 56, 57, 58, 59, 60, 61, 62, 63, \
64, 65, 66, 67, 68, 69, 70, 71, 72, 73, 74, 75, \
76, 77, 78, 79, 80, 81, 82, 83, 84, 85, 86, 87, \
88, 89, 90, 91, 92, 93, 94, 95, 96, 97, 98, 99, \
100, 101, 102, 103, 104, 105, 106, 107, 108, 109, \
110, 111, 112, 113}
#define CONFIG_SYS_NAND_ECCSIZE 512
#define CONFIG_SYS_NAND_ECCBYTES 14
#define CONFIG_SYS_NAND_ONFI_DETECTION
#define CONFIG_NAND_OMAP_ECCSCHEME OMAP_ECC_BCH8_CODE_HW
#define CONFIG_SYS_NAND_U_BOOT_OFFS 0x00100000/*0x000c0000*/
/* NAND: SPL related configs */
#ifdef CONFIG_SPL_OS_BOOT
#define CONFIG_SYS_NAND_SPL_KERNEL_OFFS 0x00200000 /* kernel offset */
#endif
#endif /* !CONFIG_NAND */
我将里面的128k均修改为256k后,mdtpart命令能够使用了。
device nand0 <nand.0>, # parts = 10
#: name size offset mask_flags
0: NAND.SPL 0x00040000 0x00000000 0
1: NAND.SPL.backup1 0x00040000 0x00040000 0
2: NAND.SPL.backup2 0x00040000 0x00080000 0
3: NAND.SPL.backup3 0x00040000 0x000c0000 0
4: NAND.u-boot-spl-os 0x00040000 0x00100000 0
5: NAND.u-boot 0x00100000 0x00140000 0
6: NAND.u-boot-env 0x00040000 0x00240000 0
7: NAND.u-boot-env.backup10x00040000 0x00280000 0
8: NAND.kernel 0x00800000 0x002c0000 0
9: NAND.file-system 0x3f540000 0x00ac0000 0
active partition: nand0,0 - (NAND.SPL) 0x00040000 @ 0x00000000
defaults:
mtdids : nand0=nand.0
mtdparts: mtdparts=nand.0:256k(NAND.SPL),256k(NAND.SPL.backup1),256k(NAND.SPL.backup2),256k(NAND.SPL.backup3),256k(NAND.u-boot-spl-os),1m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup1),8m(NAND.kernel),-(NAND.file-system)
但这里的这些分区是否能够进行合并,分区的大小依据是什么
另外,我进行nand write操作时,系统提示EEC错误
NAND erase: device 0 offset 0x100000, size 0x180000
Erasing at 0x240000 -- 100% complete.
OK
=> nand write 0x82000000 0x1000000 1x180000
NAND write: '1x180000' is not a number
=> nand write 0x82000000 0x1000000 0x180000
NAND write: device 0 offset 0x1000000, size 0x180000
omap-elm: uncorrectable ECC errors
omap-elm: uncorrectable ECC errors
NAND write to offset 1000000 failed -5
0 bytes written: ERROR
我前面有修改NAND_ECCPOS、ECCSIZE、ECCBYTES的大小,请问这ECC错误应该如何解决?