应用SDK7.0软件包,SD卡加载,启动内核时,log的结果显示如下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应用SDK7.0软件包,SD卡加载,启动内核时,log的结果显示如下:
你每次启动的时候都是这样的情况吗?
这里VDD_MPU的log意思是在把你的AM335x设置成为1G的主频,并相应提高电压到1.32V左右;VDD_CORE设置为1.1V,OPP100状态,log数值上是符合预期的。
你目前这个板子上面的AM335x是PG2.1的能跑在1GHz的AM335x芯片吗?看丝印的后缀是多少有没有“100”的字样。
如果不是100的话,芯片是不能跑到1GHz上的,这里的VDD_MPU设置就有问题。
如果是100的话,建议检测一下VDD_MPU的电压,看起是否有跌落到1.272V以下,1.272V是AM335x跑在1GHz的电压下限值(参考AM335x的datasheet的OPP Nitro定义)。
是否能跑1G和AM3358还是5几是没有关系的,关键是频率等级是否支持1GHz(最简单的方式就是通过丝印层来辨识)。你能看到板子上面AM335x主芯片上的料号么?比如AM3358BZCZ80。类似于这样的信息。
你说的VDD3测得是5V,这个VDD3是指TPS65910的哪个脚,接到AM335x上的哪个脚?
AM3354BZCZD80可以跑到1GHZ吗?还有这个从丝印看频率的根据是哪个文档的那部分呀?