这是我的程序
void adc_setup(void)
{
//
InitAdcAio();
InitAdc(); // For this example, init the ADC,库函数自带的初始化
AdcOffsetSelfCal();
//ad的相关配置
EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch
AdcRegs.INTSEL1N2.bit.INT1E = 1; //Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 1; //Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 5; //setup EOC5 to trigger ADCINT1 to fire
AdcRegs.ADCSOC0CTL.bit.CHSEL = 8; //set SOC0 channel select to ADCINB0;u_out
AdcRegs.ADCSOC1CTL.bit.CHSEL = 9; //set SOC1 channel select to ADCINB1;i_l
AdcRegs.ADCSOC2CTL.bit.CHSEL = 1; //set SOC2 channel select to ADCINA1;u_in
AdcRegs.ADCSOC3CTL.bit.CHSEL = 11; //set SOC3 channel select to ADCINB3;u_gnd
AdcRegs.ADCSOC4CTL.bit.CHSEL = 12; //set SOC4 channel select to ADCINB4;t1
AdcRegs.ADCSOC5CTL.bit.CHSEL = 13; //set SOC5 channel select to ADCINB5;t2
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 14; //set SOC0 start trigger on EPWM5 ,ADCSOCB, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 14; //set SOC1 start trigger on EPWM5B, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 14; //set SOC2 start trigger on EPWM5B, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 14; //set SOC3 start trigger on EPWM5B, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 14; //set SOC4 start trigger on EPWM5B, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC5CTL.bit.TRIGSEL = 14; //set SOC5 start trigger on EPWM5B, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC0CTL.bit.ACQPS = 20; //set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
AdcRegs.ADCSOC1CTL.bit.ACQPS = 20; //set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
AdcRegs.ADCSOC2CTL.bit.ACQPS = 20; //set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
AdcRegs.ADCSOC3CTL.bit.ACQPS = 20; //set SOC3 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
AdcRegs.ADCSOC4CTL.bit.ACQPS = 20; //set SOC4 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
AdcRegs.ADCSOC5CTL.bit.ACQPS = 20; //set SOC5 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
__interrupt void adc_isr(void)
{
//unsigned int pwmout;
g_adc_raw[0][g_adc_pos]= AdcResult.ADCRESULT0;
g_adc_raw[1][g_adc_pos] =AdcResult.ADCRESULT1;
g_adc_raw[2][g_adc_pos] =AdcResult.ADCRESULT2;
g_adc_raw[3][g_adc_pos] = AdcResult.ADCRESULT3;
g_adc_raw[4][g_adc_pos] = AdcResult.ADCRESULT4;
g_adc_raw[5][g_adc_pos] =AdcResult.ADCRESULT5;
g_adc_pos++;
if (g_adc_pos>=MAXADCNUM)//以下程序执行的时间应该测试出来????
{
g_adc_pos =0;
pid_all();//pid调节运算
}
else
{
//adc_seq1_start();//一个pwmb的中断中启动了adc,连续转换9次
}
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Clear ADCINT1 flag reinitialize for next SOC
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
return;
}
这是采样的结果。实际电位都是0,为什么第一组数据总是偏差很大。