This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00961:在应用GaN的高功率密度电源方案中,使用TMS320F280049的好处有哪些?

Part Number:

问: 在应用GaN的高功率密度电源方案中,使用TMS320F280049有哪些好处?

答: 

TIDA-00961 是TI的一个参考设计,它介绍了高频CrM(临界导通)模式下的图腾柱PFC,是一个简单的采用GaN实现高功率密度的电源解决方案。 TMS320F280049  是TI C2000新一代的产品,被用作TIDA-00961方案中的主控平台。因为TIDA-00961 参考设计中的开关频率可大于1MHz, TMS320F280049的100MHz CPU+FPU+TMU功能有助于实现参考设计中的3个环路控制,特别是需要闭环控制的快速ZVS环路。

TMS320F280049 的第四代PWM是在可变频率下,实现精准多相交错控制的关键因素。并且,在参考设计中,第四代PWM能够帮助实现高精度的死区时间控制。整体方案中需要进行大量的运算,而TMS320F280049 的TMU能够将计算时间缩短至1/20。

关于这个主题更多的信息, 请参考User Guide for TIDA-00961 的2.3章节 "System Design Theory" 。你也可以从TIDA-00961文件夹中,下载更多的参考设计文件 (BOM, 原理图, Gerber) 。