This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D controlCARD 功耗是多大?

Other Parts Discussed in Thread: TMS320F28379D

最近想利用TI的TMS320F28379D controlCARD 做一些相关功率部分的设计, 有以下几个问题想问下:

1. TMS320F28379D controlCARD是外部的5V供电,该卡所需的最大电流是多少,最大功耗是多少,在用户手册上没有找到?

2.采用板卡上的USB进行烧录与用controlCARD Docking Station上的JTAG烧录有什么不同,我是不是可以只用USB来进行烧录就可以啊?

3.如果我用USB来进行样机的在线仿真会有什么问题?

  • 1、controlCARD的功耗主要在芯片,可以在datasheet第52页5.5章Power Consumption Summary上找到。
    2、理论上没什么区别,都可以使用。不过个人用下来的经验觉得用外接JTAG比较好用些。
  • 我看了F28379D的datasheet 上说功耗不超过1W,但是我看到在User's guide--SPRUI76A中第二页上写到The F28379DExperimenter’s Kit shipswith a USBcableand is designedto be poweredvia USB.However,in extremecasesthe board/controlCARDmay requiremorepowerthanthe 5V @ 500mAacomputer’s USBport can provide(<0.01%of use cases).This is especiallytrue whenadditionalcircuitryhas beenaddedto the dockingstation.请问什么时候电流会大于500mA呢
  • 这个概率就万分之一,而且原文也做了部分解释:This is especially true when additional circuitry has been added to the docking station.
    更可能发生这个情况的原因是因为有附加电路连接到板子上。
  • 非常感谢你的解释,我估计功耗应该不超过2W,还有一个问题关于这个板子,今天在看controlCARD Docking Station [R4.1]原理图发现板子上通过USB的5V通过TPS79533DCQ转的3.3V没有接到DSPF28379D板上,也没有通过JTAG接口接到DSP上,那这个3.3V主要作用是什么?只是用来生成板子上的3.3V的一些基准信号吗,还有DSPF28379D Control CARD是只需要5V供电就可以了么,这个3.3只接到了JTAG上也没有接到DSP板上估计是给仿真器的副边供电,是这样的吗?

  • 1.5V/500mA应该足够了 IO口设计合理 输入输出电流比较大时 发热、功耗都比较大 所以外设要连接合理
    2.此板卡自带USB-JTAG设计模块 通过FTDI芯片实现 直接可以进行仿真调试和flash固化