This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用inspin-foc例程,遇到了问题。请求帮助。

Other Parts Discussed in Thread: MOTORWARE, BOOSTXL-DRV8323RS, BOOSTXL-DRV8323RH, LAUNCHXL-F28027F, LAUNCHXL-F28069M

TI的工程师们,好

我手头上有一块DRV8323RS的板子,从板子的电阻配置来看是用的SPI方式通信。

然后我用STM32F28069M的LAUNCHPAD和这个板子搭配,下载了官网的示例程序.

首先发现的是,这个板子和官网那个好像不一样,主要是MOS这个有变化。

然后我将下载的

替换原来motorware里的例程,导入工程后。

使用了Lab2c,来进行电机参数识别,电源电压15V,但发现运行完Voffset和Ioffset过程后

驱动板红灯就亮了,然后过程就停止了,稳压源也出现保护提示。

单独测试时发现驱动部分都是正常的,也就是6路PWM都正常。

想请问一下:
1.我手头上的这个板子还能用吗?毕竟跟官网的不一样

2.是我用的程序需要修改吗?

  • 建议您看一下链接

    e2e.ti.com/.../635499

    [FAQ] BOOSTXL-DRV8323RS and BOOSTXL-DRV8323RH InstaSPIN and MotorWare support

    您可以下载链接内的附件 qsg_hw_boostxl-drv8323rs_reva.pdfboostxldrv8323_package_mw.zip

    BOOSTXL-DRV8323RS and BOOSTXL-DRV8323RH evaluation module (EVM) can be mounted on the LAUNCHXL-F28069M or LAUNCHXL-F28027F.

    This document shows how to use BOOSTXL-DRV8323RS or BOOSTXL-DRV8323RH EVM with LaunchPadXL-C2000 to implement the evaluation or development in the latest MotorWare software.

    Attached a quick user guide and 6 example lab projects.