This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在LAUNCHXL-F280049C上能使用XDS100 USB串行端口吗?把J102上相应的信号焊接到XDS100仿真器上使用呢?

Other Parts Discussed in Thread: LAUNCHXL-F280049C

在LAUNCHXL-F280049C上能使用XDS100 USB串行端口吗?把J102上相应的信号焊接到XDS100仿真器上使用呢?

  • 你好,首先评估板自带的是XDS110的板载仿真器,没有配备外接JTAG端口。
    其次,J102是XDS110仿真器的输出端口,并不是输入口,按照文档描述,这个口是用来将评估板作为XDS110仿真器来使用时的输出口,用作仿真器功能使用时要将J101的跳帽全部去掉才可以。
    The connector J102 is provided to debug an external target with the on-board XDS110 debug probe. This
    connector allows the LaunchPad to be used as a stand-alone XDS110 debug probe. If the LaunchPad is
    being used in this manner, ensure that all of the shunts are removed from J101. This isolates the JTAG
    signals from going to the F280049C MCU.
    最后,如果你要使用外接的XDS100的话,可以连接到J101上芯片端的几个脚,上面还标注了对应的JTAG引脚信号名称。
  • 能用 需要断开所有JTAG信号 不能出现一驱动的连接方式

    错了  是多驱一

  • 板载XDS110和外接XDS100都可以正常连接,谢谢大家!

  • XDS110是独立的仿真器吗 这个110第一次看到