28375s HTQFP (PZP)100引脚封装用Ultra librarian导出AD文件空白,谁有2837x 系列100引脚的分装,急用,十分感谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
# Created by Ultra Librarian Lite 8.1.204 Copyright ? 1999-2016 # Ultra Librarian Free Reader, Accelerated-Designs Inc. StartFootprints EndFootprints StartComponents EndComponents
导入到AD16后空白
附件是导出时生成的文件
********************************************************** ************* Important Instructions Follow ************ ********************************************************** All files exported to: C:\UltraLibrarian\Library\Exported\Altium\2019-05-25_11-36-49\2019-05-25_11-36-49 To import your new library part into Altium follow these steps: 1. After running the Ultra Librarian export for the first time, you will need to copy the following files into an area where they can be accessed for all future translations. They are script files that Altium will need to be able to find. a. UL_Form.dfm b. UL_Form.pas c. UL_Import.pas d. UL_Import.prjScr 2. The above script file will need to be run from within Altium. This can be done by going to File, Open and selecting the UL_Import.PrjScr file stored above. 3. Select the UL_Form.pas file form the new project that has loaded, and then select runfrom the drop down menu. You will need to select the form again. Run the form. 3. When the script is run, it will ask you for the file name of the Ultra Librarian file to run. You should select the latest file produced with a date code (for instance 2010-02-17_23-12-34.txt). 4. The script will open a new Integraged Library project and import the Ultra Librarian data into it. When complete a message box will pop up saying that import is done. For additional information, please visit this site: http://www.accelerated-designs.com/help/Altium_import.html For a video tutorial, please visit: http://youtu.be/pih50yx9HYU Padstack "RX10p63Y57p53D0T_1" renamed to "RX10p63Y57p53D0T" Padstack "RX340p16Y340p16D0T_1" renamed to "RX340p16Y340p16D" Symbol "TMS320F28375S_PZP_100_01" renamed to "TMS320F28375S_PZ" Symbol "TMS320F28375S_PZP_100_00" renamed to "TMS320F28375S_00" Symbol "TMS320F28375S_PZP_100" renamed to "TMS320F28375S_01" Symbol "TMS320F28375S_PZP_100_01_1" renamed to "TMS320F28375S_02" Symbol "TMS320F28375S_PZP_100_A" renamed to "TMS320F28375S_03" Symbol "TMS320F28375S_PZP_100_B" renamed to "TMS320F28375S_04" Component "TMS320F28375S_PZP_100" renamed to "TMS320F28375S_PZ" Ultra Librarian Lite 8.1.204 Process Report Message - Pattern "PZP-100", entity (1286-Line) is a LINE with matching start and end points. Message - Pattern "PZP-100", entity (1288-Line) is a LINE with matching start and end points. Message - Pattern "PZP-100", entity (1290-Line) is a LINE with matching start and end points. Message - Pattern "PZP-100", entity (1292-Line) is a LINE with matching start and end points. TextStyle count: 69 Padstack count: 3 Pattern count: 1 Symbol count: 6 Component count: 1 Export Pad style "RX340p16Y340p16D" is a complex style and will be skipped. Footprint "PZP-100" requires pad style "RX340p16Y340p16D" and will be skipped. Component "TMS320F28375S_PZ" requires footprint "PZP-100" and will be skipped. Pad style "EX20Y20D10P_1" is a complex style and will be skipped.
你好,这是另一个版本,尝试一下