This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28027改用外部晶振出现问题,编译没报错,但运行不正确

Other Parts Discussed in Thread: LAUNCHXL-F28027

情况是这样的,硬件我用的是28027的开发板LAUNCHXL-F28027 C2000 Piccolo LaunchPad 。上面有12MHz的外部晶振,程序中我想改用外部晶振作为时钟源,在DSP2802x_SysCtrl.c里,我屏蔽了内部晶振初始化函数,加上了外部晶振初始化函数:

//IntOsc1Sel();
XtalOscSel ();

而XtalOscSel ()函数就是下面这个:

void XtalOscSel (void) {
EALLOW;
SysCtrlRegs.CLKCTL.bit.XTALOSCOFF = 0; // Turn on XTALOSC
SysCtrlRegs.CLKCTL.bit.XCLKINOFF = 1; // Turn off XCLKIN
SysCtrlRegs.CLKCTL.bit.OSCCLKSRC2SEL = 0; // Switch to external clock
SysCtrlRegs.CLKCTL.bit.OSCCLKSRCSEL = 1; // Switch from INTOSC1 to INTOSC2/ext clk
SysCtrlRegs.CLKCTL.bit.WDCLKSRCSEL = 1; // Switch Watchdog Clk Src to external clock
SysCtrlRegs.CLKCTL.bit.INTOSC2OFF = 1; // Turn off INTOSC2
SysCtrlRegs.CLKCTL.bit.INTOSC1OFF = 1; // Turn off INTOSC1
EDIS;

}

然后相应对PLL倍频数进行了修改。

完了之后编译成功,烧写到FLASH中没问题,但是运行就不正确。比如说采样是不对的,另外我定义的一个全局变量,在程序初始化中只对它赋值一次,后面就没有修改它的值了,但它却一直在0和所设定的值之间跳变。这些问题在我使用内部晶振作为时钟源时是不会发生的。

请问下,这是什么问题呢?改用外部晶振作为时钟源,除了上面的步骤,是不是还有什么步骤我漏了呢?