请问ECAP里面用来产生APWM的模块,捕获脉冲是从哪个GPIO口输入的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是ECAP文件配置的程序:
// TI File $Revision: /main/2 $
// Checkin $Date: March 15, 2007 16:54:36 $
//###########################################################################
//
// FILE: DSP2833x_ECap.c
//
// TITLE: DSP2833x eCAP Initialization & Support Functions.
//
//###########################################################################
// $TI Release: DSP2833x/DSP2823x C/C++ Header Files V1.31 $
// $Release Date: August 4, 2009 $
//###########################################################################
#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h" // DSP2833x Examples Include File
//---------------------------------------------------------------------------
// InitECap:
//---------------------------------------------------------------------------
// This function initializes the eCAP(s) to a known state.
//
void InitECap(void)
{
// Initialize eCAP1/2/3
//tbd...
}
//---------------------------------------------------------------------------
// Example: InitECapGpio:
//---------------------------------------------------------------------------
// This function initializes GPIO pins to function as ECAP pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
// Caution:
// For each eCAP peripheral
// Only one GPIO pin should be enabled for ECAP operation.
// Comment out other unwanted lines.
void InitECapGpio()
{
InitECap1Gpio();
#if (DSP28_ECAP2)
InitECap2Gpio();
#endif // endif DSP28_ECAP2
#if (DSP28_ECAP3)
InitECap3Gpio();
#endif // endif DSP28_ECAP3
#if (DSP28_ECAP4)
InitECap4Gpio();
#endif // endif DSP28_ECAP4
#if (DSP28_ECAP5)
InitECap5Gpio();
#endif // endif DSP28_ECAP5
#if (DSP28_ECAP6)
InitECap6Gpio();
#endif // endif DSP28_ECAP6
}
void InitECap1Gpio(void)
{
EALLOW;
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAPUD.bit.GPIO5 = 0; // Enable pull-up on GPIO5 (CAP1)
GpioCtrlRegs.GPAPUD.bit.GPIO24 = 1; // Disable pull-up on GPIO24 (CAP1)
// GpioCtrlRegs.GPBPUD.bit.GPIO34 = 0; // Enable pull-up on GPIO34 (CAP1)
// Inputs are synchronized to SYSCLKOUT by default.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAQSEL1.bit.GPIO5 = 0; // Synch to SYSCLKOUT GPIO5 (CAP1)
GpioCtrlRegs.GPAQSEL2.bit.GPIO24 = 0; // Synch to SYSCLKOUT GPIO24 (CAP1)
// GpioCtrlRegs.GPBQSEL1.bit.GPIO34 = 0; // Synch to SYSCLKOUT GPIO34 (CAP1)
/* Configure eCAP-1 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be eCAP1 functional pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 3; // Configure GPIO5 as CAP1
GpioCtrlRegs.GPAMUX2.bit.GPIO24 = 1; // Configure GPIO24 as CAP1
// GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 1; // Configure GPIO24 as CAP1
EDIS;
}
#if DSP28_ECAP2
void InitECap2Gpio(void)
{
EALLOW;
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAPUD.bit.GPIO7 = 0; // Enable pull-up on GPIO7 (CAP2)
GpioCtrlRegs.GPAPUD.bit.GPIO25 = 0; // Enable pull-up on GPIO25 (CAP2)
// GpioCtrlRegs.GPBPUD.bit.GPIO37 = 0; // Enable pull-up on GPIO37 (CAP2)
// Inputs are synchronized to SYSCLKOUT by default.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAQSEL1.bit.GPIO7 = 0; // Synch to SYSCLKOUT GPIO7 (CAP2)
GpioCtrlRegs.GPAQSEL2.bit.GPIO25 = 0; // Synch to SYSCLKOUT GPIO25 (CAP2)
// GpioCtrlRegs.GPBQSEL1.bit.GPIO37 = 0; // Synch to SYSCLKOUT GPIO37 (CAP2)
/* Configure eCAP-2 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be eCAP2 functional pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 3; // Configure GPIO7 as CAP2
GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 1; // Configure GPIO25 as CAP2
// GpioCtrlRegs.GPBMUX1.bit.GPIO37 = 3; // Configure GPIO37 as CAP2
EDIS;
}
#endif // endif DSP28_ECAP2
#if DSP28_ECAP3
void InitECap3Gpio(void)
{
EALLOW;
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAPUD.bit.GPIO9 = 0; // Enable pull-up on GPIO9 (CAP3)
GpioCtrlRegs.GPAPUD.bit.GPIO26 = 0; // Enable pull-up on GPIO26 (CAP3)
// Inputs are synchronized to SYSCLKOUT by default.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAQSEL1.bit.GPIO9 = 0; // Synch to SYSCLKOUT GPIO9 (CAP3)
GpioCtrlRegs.GPAQSEL2.bit.GPIO26 = 0; // Synch to SYSCLKOUT GPIO26 (CAP3)
/* Configure eCAP-3 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be eCAP3 functional pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 3; // Configure GPIO9 as CAP3
GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 1; // Configure GPIO26 as CAP3
EDIS;
}
#endif // endif DSP28_ECAP3
#if DSP28_ECAP4
void InitECap4Gpio(void)
{
EALLOW;
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
GpioCtrlRegs.GPAPUD.bit.GPIO11 = 0; // Enable pull-up on GPIO11 (CAP4)
// GpioCtrlRegs.GPAPUD.bit.GPIO27 = 0; // Enable pull-up on GPIO27 (CAP4)
// Inputs are synchronized to SYSCLKOUT by default.
// Comment out other unwanted lines.
GpioCtrlRegs.GPAQSEL1.bit.GPIO11 = 0; // Synch to SYSCLKOUT GPIO11 (CAP4)
// GpioCtrlRegs.GPAQSEL2.bit.GPIO27 = 0; // Synch to SYSCLKOUT GPIO27 (CAP4)
/* Configure eCAP-4 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be eCAP4 functional pins.
// Comment out other unwanted lines.
GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 3; // Configure GPIO11 as CAP4
// GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 1; // Configure GPIO27 as CAP4
EDIS;
}
#endif // endif DSP28_ECAP4
#if DSP28_ECAP5
void InitECap5Gpio(void)
{
EALLOW;
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0; // Enable pull-up on GPIO3 (CAP5)
GpioCtrlRegs.GPBPUD.bit.GPIO48 = 1; // Disable pull-up on GPIO48 (CAP5)
// Inputs are synchronized to SYSCLKOUT by default.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAQSEL1.bit.GPIO3 = 0; // Synch to SYSCLKOUT GPIO3 (CAP5)
GpioCtrlRegs.GPBQSEL2.bit.GPIO48 = 0; // Synch to SYSCLKOUT GPIO48 (CAP5)
/* Configure eCAP-5 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be eCAP5 functional pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 2; // Configure GPIO3 as CAP5
GpioCtrlRegs.GPBMUX2.bit.GPIO48 = 1; // Configure GPIO48 as CAP5
EDIS;
}
#endif // endif DSP28_ECAP5
#if DSP28_ECAP6
void InitECap6Gpio(void)
{
EALLOW;
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0; // Enable pull-up on GPIO1 (CAP6)
// GpioCtrlRegs.GPBPUD.bit.GPIO49 = 0; // Enable pull-up on GPIO49 (CAP6)
// Inputs are synchronized to SYSCLKOUT by default.
// Comment out other unwanted lines.
GpioCtrlRegs.GPAQSEL1.bit.GPIO1 = 0; // Synch to SYSCLKOUT GPIO1 (CAP6)
// GpioCtrlRegs.GPBQSEL2.bit.GPIO49 = 0; // Synch to SYSCLKOUT GPIO49 (CAP6)
/* Configure eCAP-5 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be eCAP6 functional pins.
// Comment out other unwanted lines.
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 2; // Configure GPIO1 as CAP6
// GpioCtrlRegs.GPBMUX2.bit.GPIO49 = 1; // Configure GPIO49 as CAP6
EDIS;
}
#endif // endif DSP28_ECAP6
//===========================================================================
// End of file.
//===========================================================================
这是主函数程序:
// $Boot_Table:
// GPIO87 GPIO86 GPIO85 GPIO84
// XA15 XA14 XA13 XA12
// PU PU PU PU
// ==========================================
// 1 1 1 1 Jump to Flash
// 1 1 1 0 SCI-A boot
// 1 1 0 1 SPI-A boot
// 1 1 0 0 I2C-A boot
// 1 0 1 1 eCAN-A boot
// 1 0 1 0 McBSP-A boot
// 1 0 0 1 Jump to XINTF x16
// 1 0 0 0 Jump to XINTF x32
// 0 1 1 1 Jump to OTP
// 0 1 1 0 Parallel GPIO I/O boot
// 0 1 0 1 Parallel XINTF boot
// 0 1 0 0 Jump to SARAM <- "boot to SARAM"
// 0 0 1 1 Branch to check boot mode
// 0 0 1 0 Boot to flash, bypass ADC cal
// 0 0 0 1 Boot to SARAM, bypass ADC cal
// 0 0 0 0 Boot to SCI-A, bypass ADC cal
// Boot_Table_End$
// DESCRIPTION:
// This example configures ePWM3A for:
// - Up count
// - Period starts at 2 and goes up to 1000
// - Toggle output on PRD
// eCAP1 is configured to capture the time between rising
// and falling edge of the PWM3A output.
//###########################################################################
// $TI Release: DSP2833x/DSP2823x C/C++ Header Files V1.31 $
// $Release Date: August 4, 2009 $
//###########################################################################
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#define PI 3.14159
#define Radius 0.22
#define LED1 GpioDataRegs.GPBDAT.bit.GPIO60
#define LED2 GpioDataRegs.GPBDAT.bit.GPIO61
// Configure the start/end period for the timer
#define DIR_L GpioDataRegs.GPBDAT.bit.GPIO49
#define DIR_R GpioDataRegs.GPADAT.bit.GPIO25
// Prototype statements for functions found within this file.
interrupt void ecap1_isr(void);
interrupt void ecap5_isr(void);
void InitECapture1(void);
void InitECapture5(void);
void InitLed(void);
void InitDIR(void);
// Global variables used in this example
Uint32 ECap1IntCount;
Uint32 ECap5IntCount;
Uint32 Period1 = 0;
Uint32 Period5 = 0;
Uint32 Time1[24]={0};
Uint32 Time5[24]={0};
Uint32 T_Per_L = 0;
Uint32 T_Per_R = 0;
Uint32 Turn_R = 0;
Uint32 Turn_L = 0;
float Spd_L = 0;
float Spd_R = 0;
// To keep track of which way the timer value is moving
void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();
InitLed();
InitDIR();
// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
InitECap1Gpio();
InitECap5Gpio();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.ECAP1_INT = &ecap1_isr;
PieVectTable.ECAP5_INT = &ecap5_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
InitECapture1();
InitECapture5();
// Step 5. User specific code, enable interrupts:
// Initalize counters:
ECap1IntCount = 0;
ECap5IntCount = 0;
// Enable CPU INT4 which is connected to ECAP1-4 INT:
IER |= M_INT4;
// Enable eCAP INTn in the PIE: Group 4 interrupt 1-6
PieCtrlRegs.PIEIER4.bit.INTx1 = 1;
PieCtrlRegs.PIEIER4.bit.INTx5 = 1;
// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
// Step 6. IDLE loop. Just sit and loop forever (optional):
for(;;)
{
asm("NOP");
}
}
void InitECapture1()
{
ECap1Regs.ECEINT.all = 0x0000; // Disable all capture interrupts 禁用所有中断使能寄存器
ECap1Regs.ECCLR.all = 0xFFFF; // Clear all CAP interrupt flags 清除所有CAP中断旗帜
ECap1Regs.ECCTL1.bit.CAPLDEN = 0; // Disable CAP1-CAP4 register loads 禁止在捕获事件中加载CAP1-4寄存器的时间
ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0; // Make sure the counter is stopped 计数器停止
// Configure peripheral registers
ECap1Regs.ECCTL2.bit.CAP_APWM = 0; // CAP moudle ECAP模块工作于捕捉模式
ECap1Regs.ECCTL2.bit.CONT_ONESHT = 1; // One shot 单次模式
ECap1Regs.ECCTL2.bit.STOP_WRAP = 0; // Stop at 1 events 单次模式下,在CAP1的捕捉事件发生后产生停止信号
ECap1Regs.ECCTL1.bit.CAP1POL = 0; // Rising edge CAP1上升沿捕捉
// ECap1Regs.ECCTL1.bit.CAP2POL = 0; // Falling edge
// ECap1Regs.ECCTL1.bit.CAP3POL = 0; // Rising edge
//ECap1Regs.ECCTL1.bit.CAP4POL = 0; // Falling edge
ECap1Regs.ECCTL1.bit.CTRRST1 = 1; // Difference operation 在CAP1捕获后重置计数器
// ECap1Regs.ECCTL1.bit.CTRRST2 = 1; // Difference operation
//ECap1Regs.ECCTL1.bit.CTRRST3 = 1; // Difference operation
//ECap1Regs.ECCTL1.bit.CTRRST4 = 1; // Difference operation
ECap1Regs.ECCTL2.bit.SYNCI_EN = 0; // Disable sync 屏蔽同步输入操作
ECap1Regs.ECCTL2.bit.SYNCO_SEL = 2; // Disable sync out 屏蔽同步信号输出
ECap1Regs.ECCTL1.bit.CAPLDEN = 1; // Enable CAP1-CAP4 register loads 使能在捕获事件中加载CAP1-4寄存器的时间
ECap1Regs.ECCTL1.bit.PRESCALE = 0; //输入信号不分频
ECap1Regs.ECCTL2.bit.TSCTRSTOP = 1; // Start Counter 计数器计数
ECap1Regs.ECCTL2.bit.REARM = 1; // arm one-shot 以下情况将强制为单次模式
ECap1Regs.ECEINT.bit.CEVT1 = 1; // CEVENT = interrupt 捕获事件1中断使能
}
void InitECapture5()
{
ECap5Regs.ECEINT.all = 0x0000; // Disable all capture interrupts 禁用所有中断使能寄存器
ECap5Regs.ECCLR.all = 0xFFFF; // Clear all CAP interrupt flags 清除所有CAP中断旗帜
ECap5Regs.ECCTL1.bit.CAPLDEN = 0; // Disable CAP1-CAP4 register loads 禁止在捕获事件中加载CAP1-4寄存器的时间
ECap5Regs.ECCTL2.bit.TSCTRSTOP = 0; // Make sure the counter is stopped 计数器停止
// Configure peripheral registers
ECap5Regs.ECCTL2.bit.CAP_APWM = 0; // CAP moudle ECAP模块工作于捕捉模式
ECap5Regs.ECCTL2.bit.CONT_ONESHT = 1; // One shot 单次模式
ECap5Regs.ECCTL2.bit.STOP_WRAP = 0; // Stop at 1 events 单次模式下,在CAP1的捕捉事件发生后产生停止信号
ECap5Regs.ECCTL1.bit.CAP1POL = 0; // Rising edge CAP1上升沿捕捉
//ECap5Regs.ECCTL1.bit.CAP2POL = 1; // Falling edge
// ECap5Regs.ECCTL1.bit.CAP3POL = 0; // Rising edge
//ECap5Regs.ECCTL1.bit.CAP4POL = 0; // Falling edge
ECap5Regs.ECCTL1.bit.CTRRST1 = 1; // Difference operation 在CAP1捕获后重置计数器
//ECap5Regs.ECCTL1.bit.CTRRST2 = 1; // Difference operation
//ECap5Regs.ECCTL1.bit.CTRRST3 = 1; // Difference operation
//ECap5Regs.ECCTL1.bit.CTRRST4 = 1; // Difference operation
ECap5Regs.ECCTL2.bit.SYNCI_EN = 0; // Disable sync 屏蔽同步输入操作
ECap5Regs.ECCTL2.bit.SYNCO_SEL = 2; // Disable sync out 屏蔽同步信号输出
ECap5Regs.ECCTL1.bit.CAPLDEN = 1; // Enable CAP1-CAP4 register loads 使能在捕获事件中加载CAP1-4寄存器的时间
ECap5Regs.ECCTL1.bit.PRESCALE = 0; //不分频
ECap5Regs.ECCTL2.bit.TSCTRSTOP = 1; // Start Counter 计数器计数
ECap5Regs.ECCTL2.bit.REARM = 1; // arm one-shot 以下情况将强制为单次模式
ECap5Regs.ECEINT.bit.CEVT1 = 1; //捕获事件4-1中断使能,1:使能
//ECap6Regs.ECEINT.bit.CEVT2 = 1; // CEVENT = interrupt
}
interrupt void ecap1_isr(void)
{
Uint32 i;
LED1=~LED1;
ECap1IntCount++;
Period1 = ECap1Regs.CAP1;
if (ECap1IntCount<=24)
{
Time1[ECap1IntCount-1] = Period1;
Period1 = 0;
if(ECap1IntCount==24)
{
for(i=0;i<24;i++)
{
T_Per_R = T_Per_R + Time1[i];
}
Spd_R = 2*PI*Radius/(float)T_Per_R/6.67*1000000000*60;
T_Per_R = 0;
}
}
else
{
Turn_R = Turn_R + 1;
ECap1IntCount = 0;
}
ECap1Regs.ECCLR.bit.CEVT1 = 1; //捕捉事件4~1标志,清除该位标志位
ECap1Regs.ECCLR.bit.INT = 1; //全局中断标志,清除该位标志位,不影响中断的使能
ECap1Regs.ECCTL2.bit.REARM = 1; //以下情况下将强制为单次模式:复位Mod4计数器为0,允许Mod4计数器持续计数,使能捕捉寄存器加载
// Acknowledge this interrupt to receive more interrupts from group 4
PieCtrlRegs.PIEACK.all = PIEACK_GROUP4;
}
interrupt void ecap5_isr(void)
{
Uint32 j;
LED2=~LED2;
ECap5IntCount++;
Period5 = ECap5Regs.CAP1;
if (ECap5IntCount<=24)
{
Time5[ECap5IntCount-1] = Period5;
Period5 = 0;
if(ECap5IntCount==24)
{
for(j=0;j<24;j++)
{
T_Per_L = T_Per_L + Time5[j];
}
Spd_L = 2*PI*Radius/(float)T_Per_L/6.67*1000000000*60;
T_Per_L = 0;
}
}
else
{
Turn_L = Turn_L + 1;
ECap5IntCount = 0;
}
ECap5Regs.ECCLR.bit.CEVT1 = 1; //捕捉事件4~1标志,清除该位标志位
//ECap5Regs.ECCLR.bit.CEVT2 = 1; // CEVENT = interrupt
ECap5Regs.ECCLR.bit.INT = 1; //全局中断标志,清除该位标志位,不影响中断的使能
ECap5Regs.ECCTL2.bit.REARM = 1; //以下情况下将强制为单次模式:复位Mod4计数器为0,允许Mod4计数器持续计数,使能捕捉寄存器加载
// Acknowledge this interrupt to receive more interrupts from group 4
PieCtrlRegs.PIEACK.all = PIEACK_GROUP4;
}
void InitLed(void)
{
EALLOW;
GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 0; // GPIO60 = GPIO60
GpioCtrlRegs.GPBDIR.bit.GPIO60 = 1; //Output
LED1=1;
GpioCtrlRegs.GPBMUX2.bit.GPIO61 = 0; // GPIO61 = GPIO61
GpioCtrlRegs.GPBDIR.bit.GPIO61 = 1;
LED2=1;
EDIS;
}
void InitDIR(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 0; // GPIO25 = GPIO25
GpioCtrlRegs.GPADIR.bit.GPIO25 = 0; // Intput
GpioCtrlRegs.GPBMUX2.bit.GPIO49 = 0; // GPIO49 = GPIO49
GpioCtrlRegs.GPBDIR.bit.GPIO49 = 0;
EDIS;
}
//===========================================================================
// No more.
//===========================================================================
请问捕获脉冲是从什么地方进入的?