This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Launchxl-F28069M 导入编译后Debug出现Debugger Initialization Error

Other Parts Discussed in Thread: LAUNCHXL-F28069M

Debugger Initialization Error

Cannot read system setup data from XML file C:\Users\ADMINI~1\WORKSP~1\EXAMPL~1\

Error parsing file:

Fatal Error at (0,0):An exception occurred! Type :RuntimeException,

message:The primary document entity could not be opened.

Id=C:\Users\ADMINI~1\WORKSP~1\EXAMPL~1\

不知是否是编译出现的warning没处理,才导致出现这个问题:

1、Invalid project path :Include path not found (\packages\ti\xdais).

2、null:creating ".sysmem" section with default size of 0x400: use the-heap

3、null:creating output  section  ".cio"without a SECTIONS specification

4、null:creating output  section  ".sysmem" without a SECTIONS specification

5、null:entry-point symbol other  than "-c-int00"  specified:"code-start"

6、variable "fid" was set