新买的LAUNCHXL-F28379D 开发板、TIDM-DC-DC-BUCK到手了,参考TIDM-DC-DC-BUCK的用户手册,LAUNCHXL-F28379D 的用户手册,进行9V上电,USB到了PC。但是不大知道程序如何写入LAUNCHXL-F28379D,并且按照TIDM-DC-DC-BUCK操作手顺,显示USB没有连接上,很苦恼,希望大神能给些提示。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
新买的LAUNCHXL-F28379D 开发板、TIDM-DC-DC-BUCK到手了,参考TIDM-DC-DC-BUCK的用户手册,LAUNCHXL-F28379D 的用户手册,进行9V上电,USB到了PC。但是不大知道程序如何写入LAUNCHXL-F28379D,并且按照TIDM-DC-DC-BUCK操作手顺,显示USB没有连接上,很苦恼,希望大神能给些提示。
抱歉,对TIDM-DC-DC-BUCK不太熟悉。所以单纯从LAUNCHXL-F28379D开发板的角度来说:
gw niu 说:但是不大知道程序如何写入LAUNCHXL-F28379D
烧写程序的话,用USB连接到电脑,使用uniflash或者CCS即可烧录
另外您的图片上传失败,请您以附件形式上传,谢谢
在CCS中设定了连接方式为XDS100V2,当前连接没有问题了,
但是点击Run,运行示例工程buck_F28004x时出现了下记的报错,S1为默认的111.
针对下记报错,应该在哪里进行改动呢??
C28xx_CPU1: Error occurred during flash operation: Unable to get file info from algorithm
C28xx_CPU1: Flash Programmer: Error during initialization (missing algorihtm). Operation Cancelled.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: F:\ti\controlSUITE\buck_F28004x\RELEASE\buck_F28004x.out: Load failed.
可以先进行烧写,看一下LAUNCHXL-F28379D好不好用,
但是我的初衷是想让Digital Power BoosterPack能有出力电压,进行调试仿真。