原打算实现ADC采样完了后,触发DMA把ADC的值自动传给参数,所以使用 DMA_ADCAINT1作为DMA的触发源,
但发现必须是能ADCA的中断,也就是说系统必须响应一次多余的ADCA中断后,才能触发DMA工作. 有办法能直接让
ADCA完成后自动触发DMA传送,而不必触发ADCA的中断吗?
谢谢!
jjl3
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, Susan
貌似这个例子也是enable了ADC中断的。
下面是我在程序中的配置, 我发现只要我关闭了ACDA的中断,不管在哪,
都无法触发DMA了。
EALLOW;
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER7.bit.INTx1 = 1; // Enable DMA_CH1 interrupt
//PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable ADCA1 interrupt
EDIS;
IER |= M_INT1 | M_INT7;
EINT;
ERTM;
void ConfigureADC(void)
{
// ADC
SetVREF(ADC_ADCA, ADC_EXTERNAL, ADC_VREF2P5);
EALLOW;
AdcaRegs.ADCCTL2.bit.PRESCALE = 6; // divided by four
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; // EOC interrupt pulse
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; // Powered up
DELAY_US(1000); // Wait for initialization
AdcaRegs.ADCSOC0CTL.bit.CHSEL = 2; // SOC0 will convert pin A2
AdcaRegs.ADCSOC0CTL.bit.ACQPS = 19; // sample window is 20 SYSCLK cycles
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 9; // trigger on ePWM3 SOCA
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 0; // EOC0 will set INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; // enable INT1 flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // make sure INT1 flag is cleared
EDIS;
}
void DMAInit(void)
{
// Initialize DMA
DMAInitialize();
// DMA set up for ADC
DMACH1AddrConfig(adc_buff, &AdcaResultRegs.ADCRESULT0);
// Enable the DMA channel 1 interrupt
DMACH1TransferConfig(3, 0, 1); // 1 T
// Set up MODE Register:
DMACH1ModeConfig(
DMA_ADCAINT1,
PERINT_ENABLE, // Peripheral interrupt enable
ONESHOT_DISABLE, // One burst transfer per trigger
CONT_ENABLE, // Channel re-initializes when TRANSFER_COUNT is zero and waits for the next event trigger
SYNC_DISABLE,
SYNC_SRC,
OVRFLOW_DISABLE, // Disable the overflow interrupt
SIXTEEN_BIT, // Data size in transfer
CHINT_END, // Generate interrupt to CPU at end of transfer
CHINT_ENABLE // Enables the DMA channel's CPU interrupt.
);