This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F280049CPMS在仿真器连接下无法正常bootload

以上是我的电路图

以下是问题描述:

我按照电路图将这一个部分的电路焊接好后使用XDS100V3烧录了c2000ware中的关于此芯片的LED_ex1_blinky代码,在修改了相关GPIO口后可以正常运行,接下来我修改到FLASH运行也一样可以运行,再然后问题出现了,断开仿真器上电程序无法运行,于是我在论坛上搜索和实验了许久,遇到的现象如下:

使用的是CCS8.1       仿真器是XDS100V3.

以下是现象:

1.连接仿真器烧写到RAM里与FLASH里均可以顺利运行到_c_int00以及之后的main函数块,但是两者在点击CPU RESET之后都无法正常运行到_c_int00函数。

2.我测试了我手上的28377S和28377D    LaunchPad,这两块板子无论是在RAN里还是在ROM里均可以正常运行,点击CPU RESET也可以正常运行。

以下是我的问题:

1.我的0049c的板子上GPIO24和GPIO32都是悬空的,那么在Standalone模式下默认就是从FLASH中启动,那么为什么即使在连接仿真器的情况下Bootloader都无法执行到_c_int00函数呢?