请教一个问题:tms320f28377d的4个16位adc可以分时启动ad转化吗,还是必须同时启动?我是想分时控制4个adc的启动顺序达到增加采样频率的目的,不知道能不能实现,有知道者请帮助解答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教一个问题:tms320f28377d的4个16位adc可以分时启动ad转化吗,还是必须同时启动?我是想分时控制4个adc的启动顺序达到增加采样频率的目的,不知道能不能实现,有知道者请帮助解答,谢谢!
请教一个问题:tms320f28377d的4个16位adc可以分时启动ad转换吗,还是只能同时启动?我是想分时控制4个adc的依次启动(adc1启动后,延时,此时还未出结果,就启动adc2.。。。)达到增加采样频率的目的,不知道能不能实现,有知道者请帮助解答,谢谢!
你好,我是想把ADC1、ADC2都接到一个模拟量输入上,先启动ADC1,隔1/2us再启动ADC2,如此循环,不是可以把原来1M的AD转换频率提高到2M吗,这样可以实现不?
我就是不知道如何触发才问啊,还不知道怎么开始呢,请问可以软件出发ad转换吗?
已经在另一个帖子给出了回复
struct ADCINTSOCSEL1_BITS { // bits description Uint16 SOC0:2; // 1:0 SOC0 ADC Interrupt Trigger Select Uint16 SOC1:2; // 3:2 SOC1 ADC Interrupt Trigger Select Uint16 SOC2:2; // 5:4 SOC2 ADC Interrupt Trigger Select Uint16 SOC3:2; // 7:6 SOC3 ADC Interrupt Trigger Select Uint16 SOC4:2; // 9:8 SOC4 ADC Interrupt Trigger Select Uint16 SOC5:2; // 11:10 SOC5 ADC Interrupt Trigger Select Uint16 SOC6:2; // 13:12 SOC6 ADC Interrupt Trigger Select Uint16 SOC7:2; // 15:14 SOC7 ADC Interrupt Trigger Select }; union ADCINTSOCSEL1_REG { Uint16 all; struct ADCINTSOCSEL1_BITS bit; }; struct ADCINTSOCSEL2_BITS { // bits description Uint16 SOC8:2; // 1:0 SOC8 ADC Interrupt Trigger Select Uint16 SOC9:2; // 3:2 SOC9 ADC Interrupt Trigger Select Uint16 SOC10:2; // 5:4 SOC10 ADC Interrupt Trigger Select Uint16 SOC11:2; // 7:6 SOC11 ADC Interrupt Trigger Select Uint16 SOC12:2; // 9:8 SOC12 ADC Interrupt Trigger Select Uint16 SOC13:2; // 11:10 SOC13 ADC Interrupt Trigger Select Uint16 SOC14:2; // 13:12 SOC14 ADC Interrupt Trigger Select Uint16 SOC15:2; // 15:14 SOC15 ADC Interrupt Trigger Select };
你加我微信可以吗:18820292912,或者qq:82612079