CCS版本10,JTAG是XDS220U,工程配置的器件是F28034,前天在板子上准备烧写代码时就提示
C28xx: Flash Programmer: Warning: The configured device (TMS320F28034), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
反复试了多次还是这样,一烧写就报错,然后不得已又新买了三片F28034,居然还是这情况。用targetconfig能连接板子,进行连接测试都是OK的
[Start: Texas Instruments XDS2xx USB Debug Probe]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\admin\AppData\Local\TEXASI~1\CCS\
ccs1000\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'May 7 2020'.
The library build time was '20:23:44'.
The library package version is '9.2.0.00002'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
这估计会是哪里问题啊