If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2014, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR243x Demo - LPM4.5, Device enters LPM4.5 waiting for a port
// interrupt on P1.3
//
// Description: Download and run the program. Program automatically enters
// LPM4.5 and measure the current. Use button SW2 (or P1.3) on the
// Target board to wake the device up from LPM4.5. This enables
// the LFXT oscillator and blink the LED (on P1.0).
//
// ACLK = XT1 = 32kHz, MCLK = SMCLK = default DCODIV = ~1MHz.
//
// MSP430FR2433
// -----------------
// /|\| |
// | | |
// | | XIN(P2.0)|--
// --|RST | 32768Hz
// | XOUT(P2.1)|--
// | |
// | P1.0|-->LED
// | |
// | P1.3|<---Button
//
// Ling Zhu
// Texas Instruments Inc.
// Feb 2015
// Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.0.1
//******************************************************************************
#include <msp430.h>
// Determine whether we are coming out of an LPMx.5 or a regular RESET.
if (SYSRSTIV == SYSRSTIV_LPM5WU) // MSP430 just woke up from LPMx.5
{
// Initialize XT1 32kHz crystal
P2SEL0 |= BIT0 | BIT1; // set XT1 pin as second function
do
{
CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
}
else
{
// Device powered up from a cold start.
// It configures the device and puts the device into LPM4.5
// Explicitly clear RTC control registers to disable it
// just incase if the RTC was previously enabled
RTCCTL = 0;
PMMCTL0_H = PMMPW_H; // Open PMM Registers for write
PMMCTL0_L |= PMMREGOFF; // and set PMMREGOFF
PMMCTL0_H = 0; // Lock PMM Registers
// Enter LPM4 Note that this operation does not return. The LPM4.5
// will exit through a RESET event, resulting in a re-start
// of the code.
__bis_SR_register(LPM4_bits | GIE);
}
// Now blink the LED in an endless loop.
while (1)
{
P1OUT ^= BIT0; // P1.0 = toggle
__delay_cycles(100000);
}
}