关于Hercules_Motorware_Dec2012例程,有如下几个问题:
1、电机电流AD采样是周期性触发、还是硬件触发,周期是多少,定点/浮点运算下DRV_run函数需要执行多长时间?
2、具体到不同电机,除了ENC_init、SMO_POS_init参数设置外,还要配置什么?
3、能否使用TMS570LS0714上,有没有其它教程资料?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于Hercules_Motorware_Dec2012例程,有如下几个问题:
1、电机电流AD采样是周期性触发、还是硬件触发,周期是多少,定点/浮点运算下DRV_run函数需要执行多长时间?
2、具体到不同电机,除了ENC_init、SMO_POS_init参数设置外,还要配置什么?
3、能否使用TMS570LS0714上,有没有其它教程资料?
谢谢!
关于Hercules_Motorware_Dec2012例程,有如下几个问题: 1、电机电流AD采样是周期性触发、还是硬件触发,周期是多少,定点/浮点运算下DRV_run函数需要执行多长时间? 2、具体到不同电机,除了ENC_init、SMO_POS_init参数设置外,还要配置什么? 3、能否使用TMS570LS0714上,有没有其它教程资料? 谢谢!
1 ADC转换由硬件触发,与PWM输出同步。
PWM频率为20KHz,周期为50us。算法的每个组件的CPU周期总数在下面的文档中指定
C:\ti\Hercules\MotorWare\v1.0.3.03\sw\solutions\foc_encoder_speed\boards\drv8301kit_revD\hercules\tms570ls1227\projects\ccs5\project01\docs
假设您在C:\ ti \ Hercules文件夹下安装了Hercules Motorware。
2 此Motorware程序还有一个GUI,允许您配置电机参数。这些也可以直接在软件中配置。
3 可以移植到0714,但您需要更新链接器命令文件以适应不同的flash和RAM内存大小