如下测试是用什么软件进行测试的?
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF. Test 1 Word 0: scanned out 0xFFFFFFFF and scanned in 0xFFFFFFC1. Scan tests: 1, skipped: 0, failed: 1 Do a test using 0x00000000. Test 2 Word 0: scanned out 0x00000000 and scanned in 0x0000003F. Scan tests: 2, skipped: 0, failed: 2 Do a test using 0xFE03E0E2. Test 3 Word 0: scanned out 0xFE03E0E2 and scanned in 0x80F83880. Test 3 Word 1: scanned out 0xFE03E0E2 and scanned in 0x80F838BF. Test 3 Word 2: scanned out 0xFE03E0E2 and scanned in 0x80F838BF. Test 3 Word 3: scanned out 0xFE03E0E2 and scanned in 0x80F838BF. Test 3 Word 4: scanned out 0xFE03E0E2 and scanned in 0x80F838BF. Test 3 Word 5: scanned out 0xFE03E0E2 and scanned in 0x80F838BF. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 3, skipped: 0, failed: 3 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 4 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 5 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 6