This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224的JTAG防护AJSM

Other Parts Discussed in Thread: HALCOGEN

我们想实现TMS570LS1224的JTAG防护,实现固件的读保护,烧录芯片后不让第三方通过JTAG口读取MCU内的固件信息,在芯片解释里有相关功能模块Advanced JTAG Security Module(AJSM)的简介,但是没有详细的技术文档和使用方法,谁有相关资料可以提供一下。

  • 这部分资料确实比较少,请您参考下我之前获取的使用示例

    2627.AJSM.zip

  • 我这边使用了HALCOGEN生成AJSM相关源码,生成的文件里面有个教程,我现在按照来做,但是没有成功,能否帮忙看一下问题出在哪?教程如下:
    Steps to Add AJSM Support:
    ; --------------------------
    ; 1) Generate the Visible Unlock Code using HALCoGen AJSM Tab.
    ; 2) Make sure Save Key is pressed before Generating HALCoGen Code.
    ; 3) Add Memory Section in linker file to program the ""ajsm"" data section
    ; to address location 0xF0000000.
    ;
    ; -------------------------------------
    ; Below example is for CCS Linker file
    ; -------------------------------------
    ; MEMORY
    ; {
    ; - - - - -
    ; - - - - -
    ; AJSM : org = 0xF0000000 len = 0x00000010
    ; AJSMECC : org = 0xF0040000 len = 0x00000002
    ; }
    ;
    ; SECTIONS
    ; {
    ; - - - - -
    ; - - - - -
    ; .ajsm : {} > AJSM
    ; .ajsmecc : {} > AJSMECC
    ; }
    ; 4) Build the project.
    ; 5) Make sure ECC is calculated and is part of the Image before programming
    ; Note: If ECC locations are not programmed correctly device might be
    ; locked permanently.
    ; 6) Once device programmed correctly, after reset your JTAG will be locked.
    ; 7) Below SafeTI forum Link contains the user guide for using CCS as Unlock Tool.
    ; e2eprivate.ti.com/.../3575.aspx
    ;
    ; If you don鈥檛 have access then it will tell you the link is invalid.
    ; Goto to www.ti.com/safetyanalysis to get access.
    ;
    ; 8) Use the Scan pattern in the bottom of this file for JTAG unlock.
    ; This pattern is generated when AJSM "save key" button is pressed.