你好,我想咨询一下,我用safety diagnostic library初始化了flash的ecc功能,库中有函数或者有其他办法可以软件触发ecc错误使esm模块响应吗?SL_SAELFTEST_FLASH函数可以通过参数设置实现触发ecc的错误码?
我使用的是RM48的开发板,HALCOGEN生成的驱动库,添加了safety diagnostic library
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我想咨询一下,我用safety diagnostic library初始化了flash的ecc功能,库中有函数或者有其他办法可以软件触发ecc错误使esm模块响应吗?SL_SAELFTEST_FLASH函数可以通过参数设置实现触发ecc的错误码?
我使用的是RM48的开发板,HALCOGEN生成的驱动库,添加了safety diagnostic library
您可以查看sl_esm.c
/******************************************************************************* **+--------------------------------------------------------------------------+** **| |** **| Copyright (c) 2012 Texas Instruments Incorporated |** **| ALL RIGHTS RESERVED |** **| |** **| Permission is hereby granted to licensees of Texas Instruments |** **| Incorporated (TI) products to use this computer program for the sole |** **| purpose of implementing a licensee product based on TI products. |** **| No other rights to reproduce, use, or disseminate this computer |** **| program, whether in part or in whole, are granted. |** **| |** **| TI makes no representation or warranties with respect to the |** **| performance of this computer program, and specifically disclaims |** **| any responsibility for any damages, special or consequential, |** **| connected with the use of this program. |** **| |** **+--------------------------------------------------------------------------+** *******************************************************************************/ /** * @file sl_esm.c * @version 2.4.0 * @brief File contains esm handling and interrupt handlers for esm errors * * @details This file implements interrupt handlers for the esmHigh and esmLow interrupts\n * the esm group 2 and group 1 handlers have been implemented which can be further extended\n * depending on the end application.It provides the Init function which updates the application\n * callback function and the interrupt handlers for esmHigh and esmLow interrupt.It also provides\n * API's which provide the information on the nError pin status */ /* Comments regarding various justifications for deviation from MISRA-C coding guidelines * are provided at the bottom of the file */ #include <sl_api.h> #include <sl_priv.h> #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_) #include <sl_reg_flash.h> #endif #if (FUNCTION_PROFILING_ENABLED != 0) #include <sl_sys_pmu.h> #endif #ifdef __IAR_SYSTEMS_ICC__ __fiq #endif static void sl_esm_high_intr_handler(void); #ifdef __IAR_SYSTEMS_ICC__ __irq #endif static void sl_esm_low_intr_handler(void); static void esmGroup1Handler(uint8 esmChannel); static void esmGroup2Handler(uint8 esmChannel); /*SAFETYMCUSW 298 S MR:- <APPROVED> Comment_1*/ #ifdef __IAR_SYSTEMS_ICC__ #pragma location=".noinit" static ESM_Application_Callback ESM_AppCallback; #endif #ifdef __TI_COMPILER_VERSION__ static ESM_Application_Callback ESM_AppCallback; #endif static uint32 callbackCancelCount = 0u; /*SAFETYMCUSW 61 D MR: 8.10,8.11 <APPROVED> Comment_2*/ void SL_ESM_Init(ESM_Application_Callback appCallback) { #ifdef __TI_COMPILER_VERSION__ /*SAFETYMCUSW 61 D MR: 8.10,8.11 <APPROVED> Comment_2*/ sl_vimRAM->ISR[1U] = &sl_esm_high_intr_handler; sl_vimRAM->ISR[21U] = &sl_esm_low_intr_handler; #endif #ifdef __IAR_SYSTEMS_ICC__ /*SAFETYMCUSW 61 D MR: 8.10,8.11 <APPROVED> Comment_2*/ sl_vimRAM->ISR[1] = (sl_t_isrFuncPTR)&sl_esm_high_intr_handler; sl_vimRAM->ISR[21] = (sl_t_isrFuncPTR)&sl_esm_low_intr_handler; #endif ESM_AppCallback = appCallback; } boolean SL_ESM_nERROR_Active(void) { boolean retval = FALSE; /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ if(ESM_ERROR_PIN_OFF == BF_GET(sl_esmREG->EPSR, BF_EPSF_START, BF_EPSF_LENGTH)) { retval = FALSE; } else { retval = TRUE; } return(retval); } /*SAFETYMCUSW 69 S MR:3.4 <APPROVED> Comment_3*/ #ifdef __TI_COMPILER_VERSION__ #pragma CODE_STATE(sl_esm_high_intr_handler, 32) #endif #ifdef __IAR_SYSTEMS_ICC__ __arm #endif /*SAFETYMCUSW 69 S MR:3.4 <APPROVED> Comment_3*/ #ifdef __TI_COMPILER_VERSION__ #pragma INTERRUPT(sl_esm_high_intr_handler, FIQ) #endif #ifdef __IAR_SYSTEMS_ICC__ __fiq #endif static void sl_esm_high_intr_handler(void) { register uint8 esmOffH,esmChannel; #if (FUNCTION_PROFILING_ENABLED != 0) register uint32 entrytick=0u; entrytick = _sl_pmuGetCycleCount_(); #endif /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ esmOffH = (uint8) sl_esmREG->IOFFHR; if (0u != esmOffH) { esmOffH--; #if defined(_TMS570LC43x_) || defined(_RM57Lx_) if (esmOffH >= 128u && esmOffH < 160u) { /* Group 1 channel 64 to 95 */ esmChannel = esmOffH - 64u; esmGroup1Handler(esmChannel); } else #endif if (esmOffH >= 96u) { /* Shouldn't be here... */ /* Misra C fix 477S added to make the else part non empty */ esmOffH = esmOffH; } else if (esmOffH >= 64u) { /* Group 1 channel 32 to 63 */ esmChannel = esmOffH - 32u; esmGroup1Handler(esmChannel); } else if (esmOffH >= 32u) { /* Group 2 channel 0 to 31 */ esmChannel = esmOffH - 32u; esmGroup2Handler(esmChannel); } else if (esmOffH > 0u) { /* Group 1 channel 0 to 31 */ esmChannel = esmOffH; esmGroup1Handler(esmChannel); } else { /* Shouldn't be here... */ /* Misra C fix 477S added to make the else part non empty */ esmOffH++; } } else { /* Shouldn't get here... */ /* Misra C fix 477S added to make the else part non empty */ esmOffH++; } #if (FUNCTION_PROFILING_ENABLED != 0) #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_) if ((esmChannel != ESM_G2ERR_B0TCM_ADDPAR) && (esmChannel != ESM_G2ERR_B1TCM_ADDPAR)) { #endif if(SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_entrytick == 0U ) { SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_entrytick = entrytick; SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_exittick = _sl_pmuGetCycleCount_(); } #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_) } #endif #endif } /*SAFETYMCUSW 69 S MR:3.4 <APPROVED> Comment_3*/ #ifdef __TI_COMPILER_VERSION__ #pragma CODE_STATE(sl_esm_low_intr_handler, 32) #endif #ifdef __IAR_SYSTEMS_ICC__ __arm #endif /*SAFETYMCUSW 69 S MR:3.4 <APPROVED> Comment_3*/ #ifdef __TI_COMPILER_VERSION__ #pragma INTERRUPT(sl_esm_low_intr_handler, IRQ) #endif #ifdef __IAR_SYSTEMS_ICC__ __irq #endif static void sl_esm_low_intr_handler(void) { register uint8 esmOffL,esmChannel; #if (FUNCTION_PROFILING_ENABLED != 0) register uint32 entrytick=0u; entrytick = _sl_pmuGetCycleCount_(); #endif /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ esmOffL = ((uint8)sl_esmREG->IOFFLR - (uint8)1u); #if defined(_TMS570LC43x_) || defined(_RM57Lx_) if ((esmOffL >= 128U) && (esmOffL < 160U)) { /* Group 1 channel 64 to 95 */ esmChannel = esmOffL-64u; esmGroup1Handler(esmChannel); } else { #endif if ((esmOffL >= 64U) && (esmOffL < 96U)) { /* Group 1 channel 32 to 63 */ esmChannel = esmOffL-32u; esmGroup1Handler(esmChannel); } else if( esmOffL < 32U){ /* Group 1 channel 0 to 31 */ esmChannel = esmOffL; esmGroup1Handler(esmChannel); } else { /* Shouldn't be here... */ /* Misra C fix 477S added to make the else part non empty */ esmOffL++; } #if defined(_TMS570LC43x_) || defined(_RM57Lx_) } #endif #if (FUNCTION_PROFILING_ENABLED != 0) if(SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_entrytick == 0U ) { SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_entrytick = entrytick; SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_exittick = _sl_pmuGetCycleCount_(); } #endif return; } #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_) #include "sl_reg_flash.h" #endif #ifdef __TI_COMPILER_VERSION__ #pragma WEAK(esmGroup2Handler) #endif static void esmGroup2Handler (uint8 esmChannel) { boolean cancelCallback = FALSE; register uint32 callbkParam1 = 0u, callbkParam2 = 0u, callbkParam3 = 0u; /* No need to clear ESM bit since reading ESMOFFH automatically clears the status bit */ switch (esmChannel) { #if defined(_TMS570LC43x_) || defined(_RM57Lx_) /** L2RAM Uncorrectable Error */ case ESM_G2ERR_L2RAMW_UNCORR_B: if (TRUE == SL_FLAG_GET(SRAM_ECC_ERROR_FORCING_1BIT) || TRUE == SL_FLAG_GET(SRAM_ECC_ERROR_FORCING_2BIT) ) { callbackCancelCount++; cancelCallback = TRUE; } break; /** CCMR5 CPU COMPARE Error */ case ESM_G2ERR_CCMR5_CPUCOMP_ERR: /* No additional parameters available */ callbkParam1 = 0u; /* Error is intentional due to diagnostic test - Clear the module * error */ ccmr5fREG1->_CCMSR1 = CCMR5F_CCMSR_CMPE; /* Cancel callback if this was intentional */ if (TRUE == SL_FLAG_GET(CCMR5F_CPUCOMP_ERROR_FORCING_TEST)) { if (TRUE == SL_FLAG_GET(VIM_SOFTWARE_TEST)){ vimTestFlag = TRUE; } callbackCancelCount++; cancelCallback = TRUE; } break; /** CCMR5 VIM COMPARE Error */ case ESM_G2ERR_CCMR5_VIMCOMP_ERR: /* No additional parameters available */ callbkParam1 = 0u; /* Error is intentional due to diagnostic test - Clear the module * error */ ccmr5fREG1->_CCMSR2 = CCMR5F_CCMSR_CMPE; /* Cancel callback if this was intentional */ if (TRUE == SL_FLAG_GET(CCMR5F_VIMCOMP_ERROR_FORCING_TEST)) { callbackCancelCount++; cancelCallback = TRUE; } break; /** CCMR5 Power Domain monitor Error */ case ESM_G2ERR_CCMR5_PDCOMP_ERR: /* No additional parameters available */ callbkParam1 = 0u; /* Error is intentional due to diagnostic test - Clear the module * error */ ccmr5fREG1->_CCMSR3 = CCMR5F_CCMSR_CMPE; /* Cancel callback if this was intentional */ if (TRUE == SL_FLAG_GET(CCMR5F_PDCOMP_ERROR_FORCING_TEST)) { callbackCancelCount++; cancelCallback = TRUE; } break; /** CPU1 AXIM Bus Monitor failure */ case ESM_G2ERR_CCMR5_INMCOMP_ERR: /* No additional parameters available */ callbkParam1 = 0u; /* Error is intentional due to diagnostic test - Clear the module * error */ ccmr5fREG1->_CCMSR4 = CCMR5F_CCMSR_CMPE; /* Cancel callback if this was intentional */ if (TRUE == SL_FLAG_GET(CCMR5F_INMCOMP_ERROR_FORCING_TEST)) { callbackCancelCount++; cancelCallback = TRUE; } break; #endif #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_) /** CCMR4 Compare Error */ case ESM_G2ERR_CCMR4_COMP: /* No additional parameters available */ callbkParam1 = 0u; /* Clear the module error */ ccmr4fREG1->_CCMSR = CCMR4F_CCMSR_CMPE; /* Cancel callback if this was intentional */ if (TRUE == SL_FLAG_GET(CCMR4F_ERROR_FORCING_TEST)) { callbackCancelCount++; cancelCallback = TRUE; } break; /** F021Flash Uncorrectable Error */ case ESM_G2ERR_FMC_UNCORR: if (TRUE == SL_FLAG_GET(FLASH_ADDRESS_PARITY_SELF_TEST)) { /* Disable Parity Overrun and enable only Bus Parity Enable */ sl_flashWREG->FPAROVR = F021F_FPAROVR_BUS_PAR_ENABLE; /* Clear Diagnostics enable key and Disable Diagnostics Mode */ sl_flashWREG->FDIAGCTRL &= (~(F021F_FDIAGCTRL_DIAG_EN_KEY | F021F_FDCTRL_DMODE_TEST_MODE)); callbackCancelCount++; cancelCallback = TRUE; } if (TRUE == SL_FLAG_GET(FLASH_ADDRESS_PARITY_FAULT_INJECT)) { /* Disable Parity Overrun and enable only Bus Parity Enable */ sl_flashWREG->FPAROVR = F021F_FPAROVR_BUS_PAR_ENABLE; /* Clear Diagnostics enable key and Disable Diagnostics Mode */ sl_flashWREG->FDIAGCTRL &= (~(F021F_FDIAGCTRL_DIAG_EN_KEY | F021F_FDCTRL_DMODE_TEST_MODE)); } /* Flash Un-correctable error, capture the error address */ callbkParam1 = sl_flashWREG->FUNCERRADD; /* No status to clear here */ break; /** RAM even bank (B0TCM) - uncorrectable Error */ case ESM_G2ERR_B0TCM_UNCORR: if (TRUE == SL_FLAG_GET(SRAM_RADECODE_DIAGNOSTICS)) { if (TRUE == SL_FLAG_GET(VIM_SOFTWARE_TEST)){ vimTestFlag = TRUE; } callbackCancelCount++; cancelCallback = TRUE; } callbkParam1 = sl_tcram1REG->RAMUERRADDR; /* No status to clear here */ break; /** RAM odd bank (B1TCM) - uncorrectable Error */ case ESM_G2ERR_B1TCM_UNCORR: if (TRUE == SL_FLAG_GET(SRAM_RADECODE_DIAGNOSTICS)) { callbackCancelCount++; cancelCallback = TRUE; } callbkParam1 = sl_tcram2REG->RAMUERRADDR; /* No status to clear here */ break; /** RAM even bank (B0TCM) - Address bus Parity Error */ case ESM_G2ERR_B0TCM_ADDPAR: if (TRUE == SL_FLAG_GET(SRAM_PAR_ADDR_CTRL_SELF_TEST)) { callbackCancelCount++; cancelCallback = TRUE; } callbkParam1 = sl_tcram1REG->RAMPERADDR; /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam2 = (sl_tcram1REG->RAMERRSTATUS & (TCRAM_RAMERRSTAT_WADDRPAR_FAIL | TCRAM_RAMERRSTAT_RADDRPAR_FAIL)); callbkParam3 = (uint32) 0u; /* Clear the WADDR/RADDR PAR Fail bits in TCM Regs */ break; /** RAM odd bank (B0TCM) - Address bus Parity Error */ case ESM_G2ERR_B1TCM_ADDPAR: if (TRUE == SL_FLAG_GET(SRAM_PAR_ADDR_CTRL_SELF_TEST)) { callbackCancelCount++; cancelCallback = TRUE; } callbkParam1 = sl_tcram2REG->RAMPERADDR; /* No status to clear here */ break; /** TCM - ECC live lock detect */ case ESM_G2ERR_FLASH_LIVLCK: callbkParam1 = 0u; /* No status to clear here */ break; /** Windowed Watchdog (WWD) violation */ case ESM_G2ERR_RTI_WWD_NMI: callbkParam1 = 0u; /* No status to clear here */ break; #endif default: /* nothing here - comment to avoid misra-c warning */ break; } /* Call application callback only if it's registered & if it's not masked */ /* the MSB of contains information regarding group and LSB contains the esm channel number*/ if ((0u != ESM_AppCallback) && ((boolean)(FALSE) == cancelCallback)) { (*(ESM_AppCallback))((uint32)(ESM_GRP2_MASK | esmChannel), callbkParam1, callbkParam2, callbkParam3); } return; } #ifdef __TI_COMPILER_VERSION__ #pragma WEAK(esmGroup1Handler) #endif static void esmGroup1Handler(uint8 esmChannel) { boolean cancelCallback = FALSE; register uint32 callbkParam1 = 0u, callbkParam2 = 0u, callbkParam3 = 0u; switch (esmChannel) { #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_) /** F021 Flash Correctabe error (bus1 & bus2) & non-EEPROM **/ case ESM_G1ERR_FMC_CORR: if (TRUE == SL_FLAG_GET(FLASH_ECC_TEST_MODE_1BIT)) { cancelCallback = TRUE; callbackCancelCount++; } /* Retrieve the callback parameters */ /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (sl_flashWREG->FCORERRCNT & 0x0000FFFFu); /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam2 = (sl_flashWREG->FCORERRADD); /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam3 = (sl_flashWREG->FCORERRPOS & 0x000003FFu); break; /** PLL1 Slip error **/ case ESM_G1ERR_PLL1_SLIP: /** Store the callback parameters & reset the status registers */ /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (uint32)((uint32)(sl_systemREG1->GBLSTAT & 0x00000300u) >> 8u); /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ sl_systemREG1->GBLSTAT |= (sl_systemREG1->GBLSTAT & 0x00000300u); break; /** LPOCLK Detect error */ case ESM_G1ERR_CLOCKMON_INTR: break; /** VIM Parity Error **/ case ESM_G1ERR_VIMRAM_PARITY: if (TRUE == SL_FLAG_GET(VIM_SRAM_PARITY_TEST)) { cancelCallback = TRUE; callbackCancelCount++; } /* Extract the parameters & clear the flag */ callbkParam1 = SL_VIM_ADDERR; SL_VIM_PARFLG = 1u; break; /** B0TCM ECC Correctable error **/ case ESM_G1ERR_B0TCM_CORRERR: if (TRUE == SL_FLAG_GET(SRAM_ECC_ERROR_FORCING_1BIT)) { cancelCallback = TRUE; callbackCancelCount++; } /* Call application if this error was _not_ intentional (self-test) */ /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (sl_tcram1REG->RAMSERRADDR); break; /** B1TCM ECC Correctable error **/ case ESM_G1ERR_B1TCM_CORRERR: if (TRUE == SL_FLAG_GET(SRAM_ECC_ERROR_FORCING_1BIT)) { cancelCallback = TRUE; callbackCancelCount++; } /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (sl_tcram2REG->RAMSERRADDR); /* Call application if this error was _not_ intentional (self-test) */ break; /** DCC Error */ case ESM_G1ERR_DCC1_ERR: callbkParam1 = sl_dccREG1->CNT0; callbkParam2 = sl_dccREG1->CNT1; /* Clear Error Flag */ sl_dccREG1->STAT = DCC_DCCSTAT_ERR_FLG; break; /** CCMR4 Self-Test Compare error */ case ESM_G1ERR_CCMR4_SELFTEST: /*ccmr4f selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/ /*blocking the esm application call back if the interrupt was due to a selftest*/ if (TRUE == SL_FLAG_GET(CCMR4F_ERROR_FORCING_TEST)) { callbackCancelCount++; cancelCallback = TRUE; } break; /** EEPROM Correctable Error */ case ESM_G1ERR_EEPROM_CORRERR: if (TRUE == SL_FLAG_GET(FEE_ECC_TEST_MODE_1BIT)) { cancelCallback = TRUE; callbackCancelCount++; } /* Retrieve the callback parameters */ /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (sl_flashWREG->EECORRERRADD); /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam2 = (sl_flashWREG->EECORRERRCNT); /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam3 = (sl_flashWREG->EECORRERRPOS & 0x000001FFu); break; /** EEPROM Uncorrectable Error */ case ESM_G1ERR_EEPROM_UNCORRERR: if (TRUE == SL_FLAG_GET(FEE_ECC_TEST_MODE_1BIT)) { cancelCallback = TRUE; callbackCancelCount++; } /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (sl_flashWREG->EEUNCERRADD); /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam2 = (sl_flashWREG->EESTATUS); break; #endif #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) /** PSON Compare Error */ case ESM_G1ERR_PSCON_COMPARE_ERR: /*pscon selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/ /*blocking the esm application call back if the interrupt was due to a selftest*/ /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ if ((PMM_PRCKEYREG_MKEY_ERRFCG_MODE == sl_pmmREG->PRCKEYREG) && (TRUE == SL_FLAG_GET(PSCON_ERROR_FORCING))) { cancelCallback = TRUE; } else { cancelCallback = FALSE; } /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (((sl_pmmREG->LPDDCSTAT1 & PMM_PSCON_LPDDCSTAT1_LCMPE) >> 16) /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ | (sl_pmmREG->MPDDCSTAT1 & PMM_PSCON_MPDDCSTAT1_MCMPE)); break; /** PSON Selftest Error */ case ESM_G1ERR_PSCON_SELTEST_ERR: /*pscon selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/ /*blocking the esm application call back if the interrupt was due to a selftest*/ if (TRUE == SL_FLAG_GET(PSCON_SELF_TEST)){ /* Since this is a self test related error, it's always intentionally * created by kicking off the ST in PRCKEYREG. Selftest API takes * care of clearing this error nothing needs to be done here */ cancelCallback = TRUE; callbackCancelCount++; SL_FLAG_CLEAR(PSCON_SELF_TEST); } break; #endif /** EFUSE Selftest Error */ case ESM_G1ERR_EFUSE_SELTEST_ERR: /*efuse selftests have synchronous and asynchronous modes.the efuse esm errors are not blocked by disabling interrupt during selftest*/ if ((TRUE == SL_FLAG_GET(EFUSE_SELF_TEST_STUCK_AT_ZERO))||(TRUE == SL_FLAG_GET(EFUSE_SELF_TEST_ECC))){ /* Since this is a self test related error, it's always intentionally * created by kicking off the ST in PRCKEYREG. Selftest API takes * care of clearing this error nothing needs to be done here */ cancelCallback = TRUE; callbackCancelCount++; SL_FLAG_CLEAR(EFUSE_SELF_TEST_ECC); SL_FLAG_CLEAR(EFUSE_SELF_TEST_STUCK_AT_ZERO); } break; /** EFUSE Error */ case ESM_G1ERR_EFUSE_ERR_OTHER: /*efuse has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/ /*blocking the esm application call back if the interrupt was due to a selftest*/ if (TRUE == SL_FLAG_GET(EFUSE_SELF_TEST_ECC)){ /* Since this is a self test related error, it's always intentionally * created by kicking off the ST in PRCKEYREG. Selftest API takes * care of clearing this error nothing needs to be done here */ cancelCallback = TRUE; callbackCancelCount++; SL_FLAG_CLEAR(EFUSE_SELF_TEST_ECC); } break; #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_) /** PLL2 Slip error **/ case ESM_G1ERR_PLL2_SLIP: /** Store the callback parameters & reset the status registers */ /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (uint32)((uint32)(sl_systemREG1->GBLSTAT & 0x00000300u) >> 8u); /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ sl_systemREG1->GBLSTAT |= (sl_systemREG1->GBLSTAT & 0x00000300u); break; /** DCC Error */ case ESM_G1ERR_DCC2_ERR: callbkParam1 = sl_dccREG2->CNT0; callbkParam2 = sl_dccREG2->CNT1; /* Clear Error Flag */ sl_dccREG2->STAT = DCC_DCCSTAT_ERR_FLG; break; #endif #if defined(_TMS570LC43x_) || defined(_RM57Lx_) /* CCMR5 Self-Test Compare error */ case ESM_G1ERR_CCMR5_SELFTEST: /*ccmr5f selftests have has synchronous and asynchronous modes,the * esm errors are not blocked by disabling interrupt during * selftest*/ /* blocking the esm application call back if the interrupt was due to * a selftest. * NOTE: Getting here implies that the CCMR5F has an error! */ if ((TRUE == SL_FLAG_GET(CCMR5F_CPUCOMP_SELF_TEST)) || (TRUE == SL_FLAG_GET(CCMR5F_VIMCOMP_SELF_TEST)) || (TRUE == SL_FLAG_GET(CCMR5F_PDCOMP_SELF_TEST)) || (TRUE == SL_FLAG_GET(CCMR5F_INMCOMP_SELF_TEST))) { /* clear the ESM Status flag */ BIT_SET(sl_esmREG->SR1[0], BIT(ESM_G1ERR_CCMR5_SELFTEST)); callbackCancelCount++; cancelCallback = TRUE; } break; case ESM_G1ERR_CCMR5_OPERATING_STATUS: callbackCancelCount++; cancelCallback = TRUE; sl_esmREG->SR7[0] = GET_ESM_BIT_NUM(ESM_G1ERR_CCMR5_OPERATING_STATUS); break; case ESM_G1ERR_DMA_ECC_SBERR: if(TRUE == SL_FLAG_GET(DMA_ECC_TEST_MODE_1BIT)) { callbackCancelCount++; cancelCallback = TRUE; } break; case ESM_G1ERR_DMA_ECC_UNCORR: if(TRUE == SL_FLAG_GET(DMA_ECC_TEST_MODE_2BIT)) { callbackCancelCount++; cancelCallback = TRUE; } break; case ESM_G1ERR_CAN1_ECC_SBERR: case ESM_G1ERR_CAN2_ECC_SBERR: case ESM_G1ERR_CAN3_ECC_SBERR: case ESM_G1ERR_CAN4_ECC_SBERR: if(TRUE == SL_FLAG_GET(CAN_ECC_TEST_MODE_1BIT)) { callbackCancelCount++; cancelCallback = TRUE; } break; case ESM_G1ERR_CAN1_ECC_UNCORR: case ESM_G1ERR_CAN2_ECC_UNCORR: case ESM_G1ERR_CAN3_ECC_UNCORR: case ESM_G1ERR_CAN4_ECC_UNCORR: if(TRUE == SL_FLAG_GET(CAN_ECC_TEST_MODE_2BIT)) { callbackCancelCount++; cancelCallback = TRUE; } break; case ESM_G1ERR_SPI1_ECC_SBERR: case ESM_G1ERR_SPI2_ECC_SBERR: case ESM_G1ERR_SPI3_ECC_SBERR: case ESM_G1ERR_SPI4_ECC_SBERR: case ESM_G1ERR_SPI5_ECC_SBERR: if(TRUE == SL_FLAG_GET(MIBSPI_ECC_TEST_MODE_1BIT)) { callbackCancelCount++; cancelCallback = TRUE; } break; case ESM_G1ERR_SPI1_ECC_UNCORR: case ESM_G1ERR_SPI2_ECC_UNCORR: case ESM_G1ERR_SPI3_ECC_UNCORR: case ESM_G1ERR_SPI4_ECC_UNCORR: case ESM_G1ERR_SPI5_ECC_UNCORR: if(TRUE == SL_FLAG_GET(MIBSPI_ECC_TEST_MODE_2BIT)) { callbackCancelCount++; cancelCallback = TRUE; } break; case ESM_G1ERR_PSCON_COMPARE_ERR: /*pscon selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/ /*blocking the esm application call back if the interrupt was due to a selftest*/ if ((PMM_PRCKEYREG_MKEY_ERRFCG_MODE == sl_pmmREG->PRCKEYREG) && (TRUE == SL_FLAG_GET(PSCON_ERROR_FORCING))) { cancelCallback = TRUE; } else { cancelCallback = FALSE; } callbkParam1 = ((sl_pmmREG->LPDDCSTAT1 & PMM_PSCON_LPDDCSTAT1_LCMPE) >> 16); break; case ESM_G1ERR_PSCON_SELTEST_ERR: /*pscon selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/ /*blocking the esm application call back if the interrupt was due to a selftest*/ if (TRUE == SL_FLAG_GET(PSCON_SELF_TEST)){ /* Since this is a self test related error, it's always intentionally * created by kicking off the ST in PRCKEYREG. Selftest API takes * care of clearing this error nothing needs to be done here */ cancelCallback = TRUE; callbackCancelCount++; SL_FLAG_CLEAR(PSCON_SELF_TEST); } break; /** PLL1 Slip error **/ case ESM_G1ERR_PLL1_SLIP: /** Store the callback parameters & reset the status registers */ /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ callbkParam1 = (uint32)((sl_systemREG1->GBLSTAT & 0x00000300u) >> 8u); /*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/ sl_systemREG1->GBLSTAT |= (sl_systemREG1->GBLSTAT & 0x00000300u); break; /** PLL2 Slip error **/ case ESM_G1ERR_PLL2_SLIP: /** No callback parameters - error cause not defined in device TRM */ break; #endif default: /* nothing here - comment to avoid misra-c warning */ break; } /* Call application callback only if it's registered & if it's not masked */ /* the MSB of contains information regarding group and LSB contains the esm channel number*/ if ((0u != ESM_AppCallback) && ((boolean)(FALSE) == cancelCallback)) { (*(ESM_AppCallback))((uint32)(ESM_GRP1_MASK|esmChannel), callbkParam1, callbkParam2, callbkParam3); } return; } /*Comment_1: * "Reason - Needed"*/ /*Comment_2: * "This function will be called by application so not static"*/ /*Comment_3: * "Reason - used for creation of code section for interrupt handler"*/ /*Comment_4: * "Reason - FALSE_POSITIVE The rule requires that the expression should be * guaranteed to have the same value regardless of the order in which the operands within the expression are evaluated. * This usually means no more than one volatile access occuring in the expression.The recommendation that simple * assignments should be used is intended to be restricted to simple assignments of the form x = v and not * "simple assignments" according to the ISO definition. However, the recommendation does not have to be followed * in order to be compliant with the rule. You should implement the rule (the value should be independent of the * evaluation order) for compliance purposes and you might choose to issue a warning for non-simple assignments * or you might choose to ignore them."*/