This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430F413 请问喂狗语句

Other Parts Discussed in Thread: MSP430F413
 你好,关于喂狗语句 ,问题如下,谢谢!
1、  MCU是msp430F413,使用外部晶振32K,看门狗定时器设为1S一次,请问喂狗语句是这句:WDT_ARST_1000,是吗?
      部分程序如下:
  WDTCTL = WDT_ADLY_1000;  //   // WDT 1 s, ACLK, interval timer
  __bis_SR_register(LPM3_bits + GIE);       // Enter LPM3 w/interrupt
  while(1)
  {
     WDT_ARST_1000;   /* 1000ms  " */
  }
2、WDT 定时设置与对应喂狗语句,是不是这样?
  (定时设置)                      (喂狗语句)
 WDT_ADLY_1000    :   WDT_ARST_1000
 WDT_ADLY_250   :    WDT_ARST_250
 WDT_ADLY_16    :    WDT_ARST_16
 WDT_ADLY_1_9  :    WDT_ARST_1_9
  • 1、WDT_ARST_1000是设置看门狗计时周期的语句,具体的周期时间和选用的时钟频率有关系。是2的15次方的时钟数。

    2、喂狗一般是用:WDTCTL =WDT_ARST_1000+WDTCNTCL;

  • 1、使用外部晶振32K,工作频率在1MHZ,

    SCFQCTL = SCFQ_1M; // 1MHZ fMCLK=32*fACLK */
    FLL_CTL0 |= XCAP14PF; // Configure load caps Set load cap for 32k xtal XIN Cap = XOUT Cap = 14pf */

    2、可以调用250mS一次来喂狗吗,?  谢谢!:WDTCTL =WDT_ARST_250+WDTCNTCL;   //250ms

  • 有相关例程的,您可以看一下(用WDT的定时模式来定时250ms翻转P5.1)

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2012, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP-FET430P410 Demo - WDT, Toggle P5.1, Interval Overflow ISR, 32kHz ACLK
    //
    //  Description: Toggle P5.1 using WDT configured for Interval Timer mode.
    //  Interrupt toggles LED every 250ms based on 32kHz ACLK WDT clock source.
    //  ACLK = LFXT1 = 32768Hz, MCLK = SMCLK = default DCO = 32 x ACLK = 1048576Hz
    //  //* An external watch crystal between XIN & XOUT is required for ACLK *//	
    //
    //		  MSP430F413
    //             -----------------
    //         /|\|              XIN|-
    //          | |                 | 32kHz
    //          --|RST          XOUT|-
    //            |                 |
    //            |             P5.1|-->LED
    //
    //  M. Buccini
    //  Texas Instruments Inc.
    //  Feb 2005
    //  Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.21A
    //*****************************************************************************
    #include <msp430.h>
    
    int main(void)
    {
      WDTCTL = WDT_ADLY_250;                    // WDT 250ms, ACLK, interval timer
      FLL_CTL0 |= XCAP14PF;                     // Configure load caps
      IE1 |= WDTIE;                             // Enable WDT interrupt
      P5DIR |= 0x02;                            // Set P5.1 to output direction
    
      __bis_SR_register(LPM3_bits + GIE);       // Enter LPM3 w/interrupt
    }
    
    // Watchdog Timer interrupt service routine
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=WDT_VECTOR
    __interrupt void watchdog_timer(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(WDT_VECTOR))) watchdog_timer (void)
    #else
    #error Compiler not supported!
    #endif
    {
      P5OUT ^= 0x02;                            // Toggle P5.1 using exclusive-OR
    }