This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553的ADC10外部参考电压配置

在使用ADC10的时候,准备外接参考电压VEref+

数据手册显示 将1.4配置为ADC10的采样通道 和 将1.4配置为外接参考电压输入通道 两种功能的配置方法是一样的 ,那msp430该怎么区分我到底是想将1.4配置为输入通道还是外接参考电压?
还有如果按照这样配置了P1.4作为外部参考电压输入,将P1.2作为采样输入,那么ADC10AE0 = BIT2+ BIT4; 但是INCH该选哪个呢?

想用msp430测100mV以内的信号,把ADC10外接一个150mV的参考电压,这样分辨率就能达到150/1023mV吗?