This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问BT-MSPAUDSOURCE Tools Bluetooth and MSP430 Audio开发板(MSP430F5229)的系统初始化C代码的编写

Other Parts Discussed in Thread: MSP430F5229

大家好:

    我们购买了BT-MSPAUDSOURCE Tools Bluetooth and MSP430 Audio开发板(MSP430F5229),请教系统初始化代码的编写:

例如:厡代码如下:

      WDTCTL = WDTPW + WDTHOLD;
      SCFI0 |= FN_2;
      FLL_CTL0 |= XCAP18PF;
      SCFQCTL = 127;  // 32768*128=4194304*/

 

我们希望使用DDS芯片AD9954模块!

辛苦了

            

  • 大家好:
    我们的接线对应表如下:
    数据到寄存 寄存器设定 幅度斜率 幅度斜率 外同步 CPU控制信号系统时针
    控制点
    名称 1-UPDATE 48-PS1 47-PS0 46-OSK 45-CLK 42-IN 41-SDIO 40-SCLK 39-CS
    AD9954 DEMO P1-1 P1-3 P1-5 P1-7 P2-1 P2-2 P1-9 P1-11 P1-13
    MSP430F5229 DEMO P7.5 P1.2 P1.1 P6.4 P5.2 P2.6 P2.5 P2.4 P7.1
  • 您现在是想使用AD9954开发板?为何需要两个板子联调呢?

    您可以用SPI连接MSP430 和AD9954,具体的AD9954配置参数建议您去模拟版块问一下相关的工程师
  • 您好:

        我们希望借用MSP430驱动AD9954的成熟代码, MSP430上运行的C代码下:

        WDTCTL = WDTPW + WDTHOLD;  //stop watchdog timer

        SCFI0 |= FN_2;                                   //系统时钟频率积分器

        FLL_CTL0 |= XCAP18PF;                 //配置内部晶振

        SCFQCTL = 127;  // 32768*128=4194304, 系统时钟频率控制寄存器 4.19M

    您看能帮在MSP430F5229开发板上改写这段初始化程序吗?

  • 大家早晨好:

        我们移植了“蓝牙和MSP430音频参考设计”里的A3DPDemo_SNK里的参考代码,并且连线正常;AD9954仍然不工作, 为什么?

        代码如下:

        

    int main(void) {  

        /* Turn off the watchdog timer                                       */

       WDTCTL = WDTPW | WDTHOLD;

       /* Configure the hardware for its intended use.                      */  

      HAL_ConfigureHardware();

       /* Enable interrupts and call the main application thread.           */   

      __enable_interrupt();

    #if 0

       MainThread();   /* MainThread should run continously, if it exits an error occured.  */   

     

      while(1)    {

          HAL_LedToggle(0);

          BTPS_Delay(100);

     }

    #else

            msec_s(1);

            AD9954_Initial();

            msec_s(1);

            while(1)

            {

    #if 0

                AD9954_SETFRE(10000.0);  //        

                SET_AD9954_PS0; // 

                LINEARSWEEP(1.0,100000.0);

                msec_s(1); // 

                CLR_AD9954_PS0;

    #else

                AD9954_SETFRE(1931.0);

                SET_AD9954_PS0;

                LINEARSWEEP(1.0,1931.0);

                msec_s(1);

                CLR_AD9954_PS0;

    #endif

            }

    #endif

    }

  • 但看代码看不出来的。

    建议用逻辑分析仪抓取一下时序,然后和AD9954的时序要求做下对比。就能找出原因了。

  • 大家好:

        为了提高AD9954的使用效率, 我们连线如下:

                         40 -SCLK 连 MSP430的P4.0-UCA1CLK

                         41-SDIO连 MSP430的P4.1-UCB1SDA

                         38-SDO连 MSP430的P4.2-USB1SCL

     

    请问:如果我们希望进行串口的调试(打印输出),该怎么处理?