MSP430F6736 LPM3.5模式

使用MSP430F6736,想使用LPM3.5模式,官网上例程无LPM3.5的相关配置,是否相关例程呢?如何进入。以及使用LPM3.5模式下与LPM3模式有无特别需要注意的。

3 个回复

  • 参考下其他型号的例程

    //******************************************************************************
    //   MSP430F665x Demo - LPM4.5, Backup RAM
    //
    //   Description: Board is setup to first init all ports, setup for P1.4 lo/hi
    //         transition interrupt, and start XT1 for setting BAKMEM registers.
    //         After registers are written, XT1 is disabled, and LPM4.5 is entered.
    //         Upon a lo/hi transition to P1.4, the device will awaken from LPM4.5
    //         and attempt to verify if the contents remain as they were programmed
    //         previous to entering LPM4.5. If so, the LED is lit, if not, the LED 
    //         will blink quickly. If the device was not properly put into LPM4.5 
    //         (see NOTE) before the transition was made, the LED will blink slowly
    //  NOTE: A backup supply is not required since backup is disabled by setting 
    //        the BAKDIS bit. 
    //	
    //
    //   NOTE: This code example was tested on the MSP-TS430PZ100USB Rev1.2 board.
    //         To get proper execution of this code example, first switch the JP3
    //         to external power, and force 3.0V on the VCC pin. Remove JP1 and set
    //         a multimeter on current reading to ensure proper entrance/exit of 
    //         LPM4.5. Now build the code example and program the device via the 
    //         Debug button. Press "Run" then "Terminate All" buttons. Detatch the 
    //         JTAG interface with the FET from the board. You should read around
    //         0.38uA current through JP1. Attatch a jumper wire from P1.4 (Pin 38)
    //         to Vcc, to trigger a lo/hi transition. The LED on the board should 
    //         light up, signifying a successful verificaiton of the programmed
    //         values for all four BAKMEM registers.
    //
    //  MCLK = SMCLK = default DCO~1MHz
    //
    //                MSP430F665x
    //             -----------------
    //         /|\|                 |
    //          | |                 |
    //          --|RST              |
    //      /|\   |                 |
    //       --o--|P1.4         P1.0|-->LED
    //      \|/
    //
    //   P. Thanigai
    //   Texas Instruments Inc.
    //   May 2012
    //   Built with IAR Embedded Workbench Version: 5.40 & CCS V5.2
    //******************************************************************************
    #include <msp430.h>
    
    void Board_Init(void);
    void EnterLPM45(void);
    void WakeUpLPM45(void);
    void SetBAKMEM(void);
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
      
      if(SYSRSTIV == 0x08)
      {
        WakeUpLPM45();
        P1DIR |= BIT0;                          // P1.0 Output
        // read backup RAM. if values match, turn on LED. else, clear LED.
        if((BAKMEM0==0x0000)&&(BAKMEM1==0x1111)&&(BAKMEM2==0x2222)&&(BAKMEM3==0x3333))
        {
          while(1)
            P1OUT |= BIT0;                      // all values match, turn on LED
        }
        else
        {
          while(1)                              // Blink LED fast if values don't 
          {                                     // all match
            P1OUT ^= BIT0;
            __delay_cycles(20000);
          }
        }
      }
      
      Board_Init();
      SetBAKMEM();
      EnterLPM45();
    
      P1DIR |= BIT0;                            // Code should NOT go here
      while(1)                                  // Blink LED slow if not an LPM4.5
      {                                         // Wakeup condition
        P1OUT ^= BIT0;
        __delay_cycles(500000);
      }
    
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=PORT1_VECTOR
    __interrupt void Port1_ISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(PORT1_VECTOR))) Port1_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      PMMCTL0_H = PMMPW_H;                      // open PMM
      PM5CTL0 &= ~LOCKIO;                       // Clear LOCKBAK and enable ports
      PMMCTL0_H = 0x00;                         // close PMM
    
      P1IFG &= ~BIT4;                           // Clear P1.4 IFG
      __bic_SR_register_on_exit(LPM4_bits);     // Exit LPM4.5
      __no_operation();
    }
    
    void Board_Init(void)
    {
      // Port Configuration
      P1OUT = 0x00;P2OUT = 0x00;P3OUT = 0x00;P4OUT = 0x00;P5OUT = 0x00;P6OUT = 0x00;
      P7OUT = 0x00;P8OUT = 0x00;P9OUT = 0x00;PJOUT = 0x00;
      P1DIR = 0xFF;P2DIR = 0xFF;P3DIR = 0xFF;P4DIR = 0xFF;P5DIR = 0xFF;P6DIR = 0xFF;
      P7DIR = 0xFF;P8DIR = 0xFF;P9DIR = 0xFF;PJDIR = 0xFF;
    
      // P1.4 Interrupt Configuration
      P1IES &= ~BIT4;                           // P1.4 Lo/Hi edge
      P1IE = BIT4;                              // P1.4 interrupt enabled
      P1IFG = 0;                           		// P1.4 IFG cleared
    
      // Disable VUSB LDO and SLDO
      USBKEYPID   =     0x9628;                 // set USB KEYandPID to 0x9628 
                                                // enable access to USB config reg
      USBPWRCTL &= ~(SLDOEN+VUSBEN);            // Disable the VUSB LDO and the SLDO
      USBKEYPID   =    0x9600;                  // disable access to USB config reg
      __delay_cycles(10000);                    // settle FLL
    }
    
    void EnterLPM45(void)
    {
      __enable_interrupt();
      // Turn off Clock for LPM4.5 operation
      UCSCTL6 |= XT1OFF;                        // XT1 Off  
      BAKCTL |= BAKDIS;                         // Supply power from Vcc, Vbat disabled
      PMMCTL0_H = PMMPW_H;                      // Open PMM Registers for write and set
      PMMCTL0_L |= PMMREGOFF;                   // PMMREGOFF
      __bis_SR_register(LPM4_bits);             // Enter LPM4.5 mode with interrupts
      __no_operation();                         // enabled
    }
    
    void WakeUpLPM45(void)
    {
      PMMCTL0_H = PMMPW_H;                      // open PMM
      PM5CTL0 &= ~LOCKIO;                       // Clear LOCKIO and enable ports
      PMMCTL0_H = 0x00;                         // close PMM
    
      // Restore Port settings
      P1OUT = 0x00;P2OUT = 0x00;P3OUT = 0x00;P4OUT = 0x00;P5OUT = 0x00;P6OUT = 0x00;
      P7OUT = 0x00;P8OUT = 0x00;P9OUT = 0x00;PJOUT = 0x00;
      P1DIR = 0xFF;P2DIR = 0xFF;P3DIR = 0xFF;P4DIR = 0xFF;P5DIR = 0xFF;P6DIR = 0xFF;
      P7DIR = 0xFF;P8DIR = 0xFF;P9DIR = 0xFF;PJDIR = 0xFF; 
      
      while(BAKCTL & LOCKBAK)                   // Unlock backup sub system
         BAKCTL &= ~(LOCKBAK);   
    }
    
    void SetBAKMEM(void)
    {
      // Set backup RAM values
      BAKMEM0 = 0x0000;
      BAKMEM1 = 0x1111;
      BAKMEM2 = 0x2222;
      BAKMEM3 = 0x3333;
      
    }
    


    昵称:灰小子     qq:1358611172

  • //******************************************************************************
    //   MSP430F66x Demo - RTC_B, LPM3.5, & alarm
    //
    //   Description: The RTC_B module is used to set the time, start RTC operation,
    //   and read the time from the respective RTC registers. Software will set the
    //   original time to 11:59:45 am on Friday June 22,2012. Then the RTC will
    //   be activated through software, and an alarm will be created for the next 
    //   minute (12:00:00 pm). The device will then enter LPM3.5 awaiting
    //   the event interrupt. Upon being woken up by the event, the LED on the board
    //   will be set. 
    //
    //   NOTE: This code example was created and tested using the MSP-TS430PZ100USB
    //   Rev1.2 board. To ensure that LPM3.5 is entered properly, upon opening the 
    //   debug window either hit the "Run Free" button on the dropdown menu next to 
    //   the run button if you are using CCS, or make sure to check that the 
    //   "Release JTAG on GO" option is selected if you are using IAR. 
    //   Also ensure Vcc is tied to Vbat if no backup supply is used
    //
    //  //* An external watch crystal on XIN XOUT is required for ACLK *//	
    //   ACLK = 32.768kHz, MCLK = SMCLK = default DCO~1MHz
    //
    //                MSP430F66xx
    //             -----------------
    //         /|\|              XIN|-
    //          | |                 | 32kHz
    //          --|RST          XOUT|-
    //            |                 |
    //            |             P1.0|--> LED
    //            |            Vbat |---
    //            |                 |  |
    //            |            Vcc  |---
    //   P. Thanigai
    //   Texas Instruments Inc.
    //   May 2012
    //   Built with IAR Embedded Workbench Version: 5.40 & CCS V5.2
    //*****************************************************************************
    #include <msp430.h>
    
    void Board_Init(void);
    void RTC_Init(void);
    void EnterLPM35(void);
    void WakeUpLPM35(void);
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
      if(SYSRSTIV == 0x08) 
      {
        // When woken up from LPM3.5, reinit
        WakeUpLPM35();
        // If woken up at noon, set LED
        if((RTCHOUR == 0x12)&&(RTCMIN == 0x00)&&(RTCSEC == 0x00))
        {
          P1OUT |= BIT0;
          P1DIR |= BIT0;
          while(1);
        }
        // If values do not match, blink LED fast
        else
        {
          while(1)                                  // continuous loop
          {
            P1OUT ^= BIT0;                          // XOR P1.0
            __delay_cycles(20000);                  // Delay
          }
        }
      }
      
      // Init board & RTC, then enter LPM3.5
      Board_Init();
      RTC_Init();
      EnterLPM35();
      
      // Code should not get here
      // Blink LED slowly if LPM3.5 not entered properly
      WakeUpLPM35();
      while(1)
      {
        P1OUT ^= BIT0;                          // XOR P1.0
        __delay_cycles(200000);                 // Delay
      }
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=RTC_VECTOR
    __interrupt void RTCISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(RTC_VECTOR))) RTCISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      PMMCTL0_H = PMMPW_H;                      // open PMM
      PM5CTL0 &= ~LOCKIO;                       // Clear LOCKBAK and enable ports
      PMMCTL0_H = 0x00;                         // close PMM
    
      RTCCTL0 &= ~RTCTEVIFG;
      __bic_SR_register_on_exit(LPM4_bits);     // Exit LPM4.5
      __no_operation();
    }
    
    void Board_Init(void)
    {
      // Port Configuration
      P1OUT = 0x00;P2OUT = 0x00;P3OUT = 0x00;P4OUT = 0x00;P5OUT = 0x00;P6OUT = 0x00;
      P7OUT = 0x00;P8OUT = 0x00;P9OUT = 0x00;PJOUT = 0x00;
      P1DIR = 0xFF;P2DIR = 0xFF;P3DIR = 0xFF;P4DIR = 0xFF;P5DIR = 0xFF;P6DIR = 0xFF;
      P7DIR = 0xFF;P8DIR = 0xFF;P9DIR = 0xFF;PJDIR = 0xFF;
    
      // Disable VUSB LDO and SLDO
      USBKEYPID   =     0x9628;                 // set USB KEYandPID to 0x9628 
                                                // enable access to USB config reg
      USBPWRCTL &= ~(SLDOEN+VUSBEN);            // Disable the VUSB LDO and the SLDO
      USBKEYPID   =    0x9600;                  // disable access to USB config reg
      __delay_cycles(10000);                    // settle FLL
    }
    
    void RTC_Init(void)
    {
      // Setup Clock
      UCSCTL6 &= ~(XT1OFF);                     // XT1 On
      UCSCTL6 |= XCAP_3;                        // Internal load cap
      while(BAKCTL & LOCKBAK)                   // Unlock XT1 pins for operation
         BAKCTL &= ~(LOCKBAK);  
      do
      {
        UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
                                                // Clear XT2,XT1,DCO fault flags
        SFRIFG1 &= ~OFIFG;                      // Clear fault flags
      }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag
    
      // Configure RTC_B
      RTCCTL01 |= RTCTEVIE + RTCBCD + RTCHOLD;  // BCD mode, RTC hold, enable RTC 
                                                // event interrupt
      RTCYEAR = 0x2012;                         // Year = 0x2012
      RTCMON = 0x06;                            // Month = 0x06 = June
      RTCDAY = 0x22;                            // Day = 0x22 = 22nd
      RTCDOW = 0x05;                            // Day of week = 0x05 = Friday
      RTCHOUR = 0x11;                           // Hour = 0x11
      RTCMIN = 0x59;                            // Minute = 0x59
      RTCSEC = 0x45;                            // Seconds = 0x45
      
      RTCCTL1 |= RTCTEV_0;                      // Set RTCTEV for 1 minute alarm
      RTCCTL01 &= ~(RTCHOLD);                   // Start RTC calendar mode
      
      // Turn off Clock for LPM4.5 operation
      UCSCTL6 |= XT1OFF;                        // XT1 Off
    }
    
    void EnterLPM35(void)
    {
      __enable_interrupt();
      PMMCTL0_H = PMMPW_H;                      // Open PMM Registers for write
      PMMCTL0_L |= PMMREGOFF;                   // and set PMMREGOFF
      __bis_SR_register(LPM4_bits);             // Enter LPM3.5 mode with interrupts
      __no_operation();                         // enabled
    }
    
    void WakeUpLPM35(void)
    {
      PMMCTL0_H = PMMPW_H;                       // open PMM
      PM5CTL0 &= ~LOCKIO;                        // Clear LOCKBAK and enable ports
      PMMCTL0_H = 0x00;                          // close PMM
    
      // Restore Port settings
      P1OUT = 0x00;P2OUT = 0x00;P3OUT = 0x00;P4OUT = 0x00;P5OUT = 0x00;P6OUT = 0x00;
      P7OUT = 0x00;P8OUT = 0x00;P9OUT = 0x00;PJOUT = 0x00;
      P1DIR = 0xFF;P2DIR = 0xFF;P3DIR = 0xFF;P4DIR = 0xFF;P5DIR = 0xFF;P6DIR = 0xFF;
      P7DIR = 0xFF;P8DIR = 0xFF;P9DIR = 0xFF;PJDIR = 0xFF;
    
      // Restore Clock so that RTC will be read
      UCSCTL6 &= ~(XT1OFF);                     // XT1 On
      UCSCTL6 |= XCAP_3;                        // Internal load cap
      while(BAKCTL & LOCKBAK)                   // Unlock XT1 pins for operation
         BAKCTL &= ~(LOCKBAK);  
      do
      {
        UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
                                                // Clear XT2,XT1,DCO fault flags
        SFRIFG1 &= ~OFIFG;                      // Clear fault flags
      }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag  
      
      // Reconfig/start RTC
      RTCCTL01 |= RTCBCD + RTCHOLD;
      RTCCTL01 &= ~RTCHOLD;
    }
    
    


    昵称:灰小子     qq:1358611172

  • 关于LPM3.5 建议您参考下TRM内的内容

    http://www.ti.com/lit/ug/slau208q/slau208q.pdf 

    When LPMx.5 (LPM3.5 or LPM4.5) is entered, the voltage regulator of the Power Management Module(PMM) is disabled. All RAM and register contents are lost. Although the I/O register contents are lost, the I/O pin states are locked upon LPMx.5 entry. See the Digital I/O chapter for further details. Wakeup from LPM4.5 is possible from a power sequence, a RST event, or from specific I/O. Wakeup from LPM3.5 is possible from a power sequence, a RST event, RTC event, or from specific I/O.

    以及

    1.4.2 Entering and Exiting Low-Power Modes LPMx.5

     

    若是该回复回答了您的问题,请点击“确认此为答案”,谢谢

    If a post answers your question, please mark it with the "verify answer" button.