想更新CCS v5.1 但是安装后出现以下问题
Error in action ExecuteAction
Error in action ExecuteScript
list element in quotes followed by ":" instead of space while executing"::InstallJammer::actions::$component $this" while executing"$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within"::InstallJammer::ExecuteActions $action -parent $id -conditions $eval" (procedure "::InstallJammer::actions::ExecuteAction" line 35) invoked from within"::InstallJammer::actions::$component $this" while executing"$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within"::InstallJammer::ExecuteActions $action -parent $id -conditions $eval" (procedure "::InstallJammer::actions::ExecuteAction" line 35) invoked from within"::InstallJammer::actions::$component $this"Error in action ExecuteAction
list element in quotes followed by ":" instead of space while executing"::InstallJammer::actions::$component $this" while executing"$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within"::InstallJammer::ExecuteActions $action -parent $id -conditions $eval" (procedure "::InstallJammer::actions::ExecuteAction" line 35) invoked from within"::InstallJammer::actions::$component $this" while executing"$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within"::InstallJammer::ExecuteActions $action -parent $id -conditions $eval" (procedure "::InstallJammer::actions::ExecuteAction" line 35) invoked from within"::InstallJammer::actions::$component $this" while executing"$obj execute" (procedure "::InstallJammer::ExecuteActions" line 69) invoked from within"::InstallJammer::ExecuteActions $id -when $when" (procedure "::InstallJammer::RaiseEventHandler" line 93) invoked from within"::InstallJammer::RaiseEventHandler .wizard" (command bound to event)
系统是WIN XP SP3 更换系统太耗费时间和精力,希望能直接在WIN XP上解决。CCS v5.5是否需要一些运行库?请指点!
查看这个帖子 http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/289687.aspx
If a post answers your question, please mark it with the "verify answer" button.
若是回复解决了您的问题,请点击“是”确认答案。谢谢!
1 完全删除你之前安装的所有文件(包括安装文件 安装日志 注册表等)
2 在以下链接下载安装
http://processors.wiki.ti.com/index.php/Download_CCS
回复 Susan Yang:
安装日志和注册表文件在哪个位置?
回复 hongyong chen:
Hi hongyong,
你可以试试直接装V5.5的版本,CCS各版本在电脑里面是可以共存的。我的电脑里就有5.2到5。5的版本。只是这些安装版本需要安装的不同的路径下面。有的时候直接的在线更新会遇到比较多的问题。直接装另一个版本就行。
另外在安装的时候,不需要所有的控件都装,如果你只是开发430或是C2000,可以直接只选他们。这样安装起来会更快。
谢谢
ken
BR,
KEN
回复 Ken Wang:
安装时遇到这个问题,刚刚开始安装时就会弹出这个,同学的电脑安装就没问题。杀毒软件都已经关闭或者删除了,求解答。
Hi,Susan
我严格按照你说的方法,却一直安装不成功,我是利用Windows优化大师将那些全部清理掉的,之前卸载了CCS6.0,如今想重新装回去5.5,缺一直都没有结果,试了六七次都没有成功,我不知道是因为什么。
回复 guilai yin:
安装过程有什么提示吗?
安装前,各类杀毒软件、安全卫士等都要完全退出来。
昵称:灰小子
qq:1358611172
回复 灰小子:
我安装的时候并没有关闭任何杀软
你可以试试先完全卸载CCS 除了使用卸载程序,再确认一下C盘中时候有TI或CCS的文件夹,还有我的文档里面是否也有,把它们都删了。然后用杀软清一下注册列表。从前面帖子的链接中重新下一个CCS,再试试。
如果不行,请试试打一下补丁程序 如.netframework和VC++可再发行组件包?
CCS6.0以上的版本是不是不支持XP了,安装一直出错,现在只能用IAR了!!
Error in action ExecuteExternalProgram_Join
couldn't execute "C:\Users\Yin": no such file or directory
while executing
"::InstallJammer::actions::$component $this"
"$obj execute"
其他都跟楼上的差不多,都快烦死了,已经被此问题困扰了快一个月了。
之前装了CCS6.1.3,以为安装好了,结果昨晚用了依然还是不可用,唉……