FR6989调试出现问题进不了调试界面

   TI工程师您好!

             问题1: 我用FR6989调试时 I2C通讯时一使能I2C模块,程序一运行 EUSCI_B_I2C_enable(uint16_t baseAddress)时状态寄存器UCB0STATW的UCBBUSY 就置1,所以程序就运行到uint16_t EUSCI_B_I2C_isBusBusy(uint16_t baseAddress)检测到I2C总线占用就无法运行到后面的程序,

我调试很久找不出原因 I2C不论是用P3.1 P3.2或改用P4.0 P4.1都提示状态寄存器UCB0STATW的UCBBUSY 是1,。

        后来又出现下面的问题(问题2),换了3块板子调试2个MSP_FET仿真器都无法进入调试界面,请TI工程师帮我看下问题是出在哪里?非常感激!

   谢谢!

7 个回复

  • 请问您现在使用的是TI的launchpad还是您自己的板子?是使用TI例程还是自己的程序?

    若是TI例程的话,能否给出例程名称?

    If a post answers your question, please mark it with the "verify answer" button.

    若是回复解决了您的问题,请点击“是”确认答案。谢谢!

  • 关于第一个问题,您先参考一下

    e2e.ti.com/.../581257

    关于第二个问题,您是否有使用uniflash看一下,先排除板子本身硬件或者连接部分的问题。另外您的CCS/IAR版本是多少?

    If a post answers your question, please mark it with the "verify answer" button.

    若是回复解决了您的问题,请点击“是”确认答案。谢谢!

  • 1、建议提供下相关的代码,这个问题是软件原因的可能居多。或者你先运行官网的iic例程测试一下。

    2、第二个问题一般是硬件问题,建议重点检查仿真相关接口的连接情况和相关走线。


    昵称:灰小子     qq:1358611172

  • 回复 Susan Yang:

    Susan Yang :

                  您好 !程序是根据TI例程调用FR5xx6xx  I2C库

    开始我用的是MSP430FR6972 的板子自己layout 和触摸MCU msp430fr2522 I2C通讯,调试出现这个问题,I2C是根据例程例子,只是例子的I2C的SDA SCL用的是P4.0  P4.1我改为6972的P3.1 P3.0,出现这个问题我又用FR6989的板子直接运行TI例程

    也还是一样,后来又出现了问题2,FR6989是我以前另个项目的板子运行那个程序没问题的,现在运行这个程序后就无法进入调试界面,我用的IIAR 7.12的编译器,出现问题后我又用以前的IAR6.2也是一样。

    谢谢您们的回复。

  • 回复 灰小子:

    灰小子,谢谢您的回复,问题1的现象我刚回复susan Yang描述了,问题2 我用的硬件板子以前是运行是没问题的,只是前天才出现的,是否mcu IC被损坏或仿真器的JTAG接口芯片被锁死,但是仿真器我运行别的板子又没问题,只是运行F6989才会有这个问题。
  • 回复 user3883938:

    您现在是想master发送multiple bytes?driverlib内的程序可以参考下面的代码。

    总线bus一直是busy的,一直到stop bit 置位

    您不需要这样调用 isBusBusy 

    第2个问题的话,应该是您板子的硬件问题

    /* --COPYRIGHT--,BSD
     * Copyright (c) 2017, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*/
    #include "driverlib.h"
    
    //******************************************************************************
    //! This example shows how to configure the I2C module as a master for
    //! multi byte transmission in interrupt driven mode. The address of the slave
    //! module is set in this example.
    //!
    //!  Demo - EUSCI_B0 I2C Master TX multiple bytes to MSP430 Slave
    //!
    //!  Description: This demo connects two MSP430's via the I2C bus. The master
    //!  transmits to the slave. This is the MASTER CODE. It cntinuously
    //!  transmits an array of data and demonstrates how to implement an I2C
    //!  master transmitter sending multiple bytes using the USCI_B0 TX interrupt.
    //!  ACLK = n/a, MCLK = SMCLK = BRCLK = default DCO = ~1.045MHz
    //!
    //!                                /|\  /|\
    //!                MSP430FR5969    10k  10k      MSP430FR5969
    //!                   slave         |    |         master
    //!             -----------------   |    |   -----------------
    //!           -|XIN  P1.6/UCB0SDA|<-|----+->|P1.6/UCB0SDA  XIN|-
    //!            |                 |  |       |                 |
    //!           -|XOUT             |  |       |             XOUT|-
    //!            |     P1.7/UCB0SCL|<-+------>|P1.7/UCB0SCL     |
    //!            |                 |          |                 |
    //!
    //! This example uses the following peripherals and I/O signals.  You must
    //! review these and change as needed for your own board:
    //! - I2C peripheral
    //! - GPIO Port peripheral (for I2C pins)
    //! - SCL2
    //! - SDA
    //!
    //! This example uses the following interrupt handlers.  To use this example
    //! in your own application you must add these interrupt handlers to your
    //! vector table.
    //! - USCI_B0_VECTOR.
    //
    
    //******************************************************************************
    //*****************************************************************************
    //
    //Set the address for slave module. This is a 7-bit address sent in the
    //following format:
    //[A6:A5:A4:A3:A2:A1:A0:RS]
    //
    //A zero in the "RS" position of the first byte means that the master
    //transmits (sends) data to the selected slave, and a one in this position
    //means that the master receives data from the slave.
    //
    //*****************************************************************************
    #define SLAVE_ADDRESS 0x48
    
    uint8_t TXData =0;                    // Pointer to TX data
    uint8_t TXByteCtr;
    
    void main(void)
    {
        WDT_A_hold(WDT_A_BASE);
    
        //Set DCO frequency to 1MHz
        CS_setDCOFreq(CS_DCORSEL_0,CS_DCOFSEL_0);
        //Set ACLK = VLO with frequency divider of 1
        CS_initClockSignal(CS_ACLK,CS_VLOCLK_SELECT,CS_CLOCK_DIVIDER_1);
        //Set SMCLK = DCO with frequency divider of 1
        CS_initClockSignal(CS_SMCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);
        //Set MCLK = DCO with frequency divider of 1
        CS_initClockSignal(CS_MCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);
    
        // Configure Pins for I2C
        //Set P1.6 and P1.7 as Secondary Module Function Input.
        /*
    
        * Select Port 1
        * Set Pin 6, 7 to input Secondary Module Function, (UCB0SIMO/UCB0SDA, UCB0SOMI/UCB0SCL).
        */
        GPIO_setAsPeripheralModuleFunctionInputPin(
        	GPIO_PORT_P1,
        	GPIO_PIN6 + GPIO_PIN7,
        	GPIO_SECONDARY_MODULE_FUNCTION
        );
    
        /*
         * Disable the GPIO power-on default high-impedance mode to activate
         * previously configured port settings
         */
        PMM_unlockLPM5();
    
        EUSCI_B_I2C_initMasterParam param = {0};
        param.selectClockSource = EUSCI_B_I2C_CLOCKSOURCE_SMCLK;
        param.i2cClk = CS_getSMCLK();
        param.dataRate = EUSCI_B_I2C_SET_DATA_RATE_400KBPS;
        param.byteCounterThreshold = 0;
        param.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP;
        EUSCI_B_I2C_initMaster(EUSCI_B0_BASE, &param);
    
        //Specify slave address
        EUSCI_B_I2C_setSlaveAddress(EUSCI_B0_BASE,
        			SLAVE_ADDRESS
        			);
    
        //Set Master in receive mode
        EUSCI_B_I2C_setMode(EUSCI_B0_BASE,
        			EUSCI_B_I2C_TRANSMIT_MODE
        			);
    
        //Enable I2C Module to start operations
        EUSCI_B_I2C_enable(EUSCI_B0_BASE);
    
        EUSCI_B_I2C_clearInterrupt(EUSCI_B0_BASE,
        			EUSCI_B_I2C_TRANSMIT_INTERRUPT0 +
        			EUSCI_B_I2C_NAK_INTERRUPT
        			);
    
        //Enable master Receive interrupt
        EUSCI_B_I2C_enableInterrupt(EUSCI_B0_BASE,
        			EUSCI_B_I2C_TRANSMIT_INTERRUPT0 +
        			EUSCI_B_I2C_NAK_INTERRUPT
        		  );
        while(1)
        {
        __delay_cycles(1000);                   // Delay between transmissions
        TXByteCtr = 4;                          // Load TX byte counter
        TXData = 0;
    
        while (EUSCI_B_I2C_SENDING_STOP == EUSCI_B_I2C_masterIsStopSent
        		(EUSCI_B0_BASE));
    
        EUSCI_B_I2C_masterSendMultiByteStart(EUSCI_B0_BASE,
        		TXData++);
    
        __bis_SR_register(CPUOFF + GIE);        // Enter LPM0 w/ interrupts
        										// Remain in LPM0 until all data
        										// is TX'd
        										// Increment data byte
        }
    }
    
    //------------------------------------------------------------------------------
    // The USCIAB0TX_ISR is structured such that it can be used to transmit any
    // number of bytes by pre-loading TXByteCtr with the byte count. Also, TXData
    // points to the next byte to transmit.
    //------------------------------------------------------------------------------
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=USCI_B0_VECTOR
    __interrupt
    #elif defined(__GNUC__)
    __attribute__((interrupt(USCI_B0_VECTOR)))
    #endif
    void USCIB0_ISR(void)
    {
        switch(__even_in_range(UCB0IV, USCI_I2C_UCBIT9IFG))
      {
            case USCI_NONE:             // No interrupts break;
                break;
            case USCI_I2C_UCALIFG:      // Arbitration lost
                break;
            case USCI_I2C_UCNACKIFG:    // NAK received (master only)
    			//resend start if NACK
    			EUSCI_B_I2C_masterSendStart(EUSCI_B0_BASE);
                break;
            case USCI_I2C_UCTXIFG0:     // TXIFG0
                // Check TX byte counter
                if (TXByteCtr)
                {
                    EUSCI_B_I2C_masterSendMultiByteNext(EUSCI_B0_BASE, TXData++);
                    // Decrement TX byte counter
                    TXByteCtr--;
                }
                else
                {
                    EUSCI_B_I2C_masterSendMultiByteStop(EUSCI_B0_BASE);
                    // Exit LPM0
                    __bic_SR_register_on_exit(CPUOFF);
                }
                break;
            default:
                break;
      }
    }
    
    

    If a post answers your question, please mark it with the "verify answer" button.

    若是回复解决了您的问题,请点击“是”确认答案。谢谢!

  • 回复 user3883938:

    现在msp430的jtag熔丝,都是电子熔丝,都是可以使用仿真器来恢复的。所以不存在锁死的问题。
    至于mcu是不是损坏了,这个只要没有接过较高的电压或者其他恶劣情况,msp430也不太容易坏的。

    昵称:灰小子     qq:1358611172