采用FR5969芯片,仿真器是2线制连接方式,在IAR软件单步运行可以观察到P2寄存器值的变化,但是用示波器在芯片的P2.7管脚一直检测不到高低电平的变化,没有输出。
想问下
1.这种情况下 可以判断仿真器已经把程序下载到芯片了么?
2.无法检测输出波形有哪些可能的原因呢? 仿真器的连接方式或者芯片通信有冲突?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用FR5969芯片,仿真器是2线制连接方式,在IAR软件单步运行可以观察到P2寄存器值的变化,但是用示波器在芯片的P2.7管脚一直检测不到高低电平的变化,没有输出。
想问下
1.这种情况下 可以判断仿真器已经把程序下载到芯片了么?
2.无法检测输出波形有哪些可能的原因呢? 仿真器的连接方式或者芯片通信有冲突?
1 IAR调试的话,有Debug without Download和Debug with Download。需要调试并下载的话,请选择Debug with Download
2 产生方波的话,请使用PWM.在MSP430WAR内是有例程的
MSP430Ware\examples\devices\MSP430FR5xx_6xx\MSP430FR596x_MSP430FR595x_MSP430FR594x_MSP430FR586x_MSP430FR585x_MSP430FR584x_Code_Examples\C
msp430fr59xx_ta0_16以及msp430fr59xx_ta0_17等