我们客户使用MSP432P401R,目前对于芯片内部的I/O口引脚类型存在疑问,希望解答一下I/O引脚是推挽、开漏还是单纯的上下拉输入输出。
这个主要是影响到客户外围电路设计。因为如果MCU的I/O口是推挽输出,客户外部电路加入需要一个不同电压等级的功能,引脚会被强制限制在3.3V或0V,如果是开漏输出,客户通过外部上下拉电阻可能会获取一个更高范围的电压。客户希望能解答一下MCU内部,I/O口的输出电路具体实现方案。
希望获取您的帮助。
Kevin Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们客户使用MSP432P401R,目前对于芯片内部的I/O口引脚类型存在疑问,希望解答一下I/O引脚是推挽、开漏还是单纯的上下拉输入输出。
这个主要是影响到客户外围电路设计。因为如果MCU的I/O口是推挽输出,客户外部电路加入需要一个不同电压等级的功能,引脚会被强制限制在3.3V或0V,如果是开漏输出,客户通过外部上下拉电阻可能会获取一个更高范围的电压。客户希望能解答一下MCU内部,I/O口的输出电路具体实现方案。
希望获取您的帮助。
Kevin Chen
不具备推挽开漏,只有配置输入输出,以及配置上拉下拉功能,IO功能基本上跟430的类似。
这个确认可以参考头文件。
/* * ------------------------------------------- * MSP432 DriverLib - v3_21_00_05 * ------------------------------------------- * * --COPYRIGHT--,BSD,BSD * Copyright (c) 2016, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * --/COPYRIGHT--*/ #ifndef __GPIO_H__ #define __GPIO_H__ //***************************************************************************** // //! \addtogroup gpio_api //! @{ // //***************************************************************************** //***************************************************************************** // // If building with a C++ compiler, make all of the definitions in this header // have a C binding. // //***************************************************************************** #ifdef __cplusplus extern "C" { #endif #include <msp.h> #include <stdint.h> #define GPIO_PORT_P1 1 #define GPIO_PORT_P2 2 #define GPIO_PORT_P3 3 #define GPIO_PORT_P4 4 #define GPIO_PORT_P5 5 #define GPIO_PORT_P6 6 #define GPIO_PORT_P7 7 #define GPIO_PORT_P8 8 #define GPIO_PORT_P9 9 #define GPIO_PORT_P10 10 #define GPIO_PORT_PA 1 #define GPIO_PORT_PB 3 #define GPIO_PORT_PC 5 #define GPIO_PORT_PD 7 #define GPIO_PORT_PE 9 #define GPIO_PORT_PJ 11 #define GPIO_PIN0 (0x0001) #define GPIO_PIN1 (0x0002) #define GPIO_PIN2 (0x0004) #define GPIO_PIN3 (0x0008) #define GPIO_PIN4 (0x0010) #define GPIO_PIN5 (0x0020) #define GPIO_PIN6 (0x0040) #define GPIO_PIN7 (0x0080) #define GPIO_PIN8 (0x0100) #define GPIO_PIN9 (0x0200) #define GPIO_PIN10 (0x0400) #define GPIO_PIN11 (0x0800) #define GPIO_PIN12 (0x1000) #define GPIO_PIN13 (0x2000) #define GPIO_PIN14 (0x4000) #define GPIO_PIN15 (0x8000) #define PIN_ALL8 (0xFF) #define PIN_ALL16 (0xFFFF) #define GPIO_PRIMARY_MODULE_FUNCTION (0x01) #define GPIO_SECONDARY_MODULE_FUNCTION (0x02) #define GPIO_TERTIARY_MODULE_FUNCTION (0x03) #define GPIO_HIGH_TO_LOW_TRANSITION (0x01) #define GPIO_LOW_TO_HIGH_TRANSITION (0x00) #define GPIO_INPUT_PIN_HIGH (0x01) #define GPIO_INPUT_PIN_LOW (0x00) //***************************************************************************** // // Prototypes for the APIs. // //***************************************************************************** //***************************************************************************** // //! \brief This function configures the selected Pin as output pin //! //! This function selected pins on a selected port as output pins. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxDIR register and bits of \b PxSEL register. //! //! \return None // //***************************************************************************** extern void GPIO_setAsOutputPin(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function configures the selected Pin as input pin //! //! This function selected pins on a selected port as input pins. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxDIR register, bits of \b PxREN register and bits of //! \b PxSEL register. //! //! \return None // //***************************************************************************** extern void GPIO_setAsInputPin(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function configures the peripheral module function in the //! output direction for the selected pin for either primary, secondary or //! ternary module function modes //! //! This function configures the peripheral module function in the output //! direction for the selected pin for either primary, secondary or ternary //! module function modes. Accepted values for mode are //! GPIO_PRIMARY_MODULE_FUNCTION, GPIO_SECONDARY_MODULE_FUNCTION, and //! GPIO_TERTIARY_MODULE_FUNCTION //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! \param mode is the specified mode that the pin should be configured for the //! module function. //! Valid values are: //! - \b GPIO_PRIMARY_MODULE_FUNCTION //! - \b GPIO_SECONDARY_MODULE_FUNCTION //! - \b GPIO_TERTIARY_MODULE_FUNCTION //! //! Modified bits of \b PxDIR register and bits of \b PxSEL register. //! //! \return None // //***************************************************************************** extern void GPIO_setAsPeripheralModuleFunctionOutputPin( uint_fast8_t selectedPort, uint_fast16_t selectedPins, uint_fast8_t mode); //***************************************************************************** // //! \brief This function configures the peripheral module function in the input //! direction for the selected pin for either primary, secondary or ternary //! module function modes. //! //! This function configures the peripheral module function in the input //! direction for the selected pin for either primary, secondary or ternary //! module function modes. Accepted values for mode are //! GPIO_PRIMARY_MODULE_FUNCTION, GPIO_SECONDARY_MODULE_FUNCTION, and //! GPIO_TERTIARY_MODULE_FUNCTION //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! \param mode is the specified mode that the pin should be configured for the //! module function. //! Valid values are: //! - \b GPIO_PRIMARY_MODULE_FUNCTION //! - \b GPIO_SECONDARY_MODULE_FUNCTION //! - \b GPIO_TERTIARY_MODULE_FUNCTION //! //! Modified bits of \b PxDIR register and bits of \b PxSEL register. //! //! \return None // //***************************************************************************** extern void GPIO_setAsPeripheralModuleFunctionInputPin( uint_fast8_t selectedPort, uint_fast16_t selectedPins, uint_fast8_t mode); //***************************************************************************** // //! \brief This function sets output HIGH on the selected Pin //! //! This function sets output HIGH on the selected port's pin. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxOUT register. //! //! \return None // //***************************************************************************** extern void GPIO_setOutputHighOnPin(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function sets output LOW on the selected Pin //! //! This function sets output LOW on the selected port's pin. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! \return None // //***************************************************************************** extern void GPIO_setOutputLowOnPin(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function toggles the output on the selected Pin //! //! This function toggles the output on the selected port's pin. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxOUT register. //! //! \return None // //***************************************************************************** extern void GPIO_toggleOutputOnPin(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function sets the selected Pin in input Mode with Pull Down //! resistor //! //! This function sets the selected Pin in input Mode with Pull Down resistor. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxDIR register, bits of \b PxOUT register and bits of //! \b PxREN register. //! //! \return None // //***************************************************************************** extern void GPIO_setAsInputPinWithPullDownResistor(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function sets the selected Pin in input Mode with Pull Up //! resistor //! //! This function sets the selected Pin in input Mode with Pull Up resistor. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxDIR register, bits of \b PxOUT register and bits of //! \b PxREN register. //! //! \return None // //***************************************************************************** extern void GPIO_setAsInputPinWithPullUpResistor(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function gets the input value on the selected pin //! //! This function gets the input value on the selected pin. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Valid values are: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! \return One of the following: //! - \b GPIO_INPUT_PIN_HIGH //! - \b GPIO_INPUT_PIN_LOW //! \n indicating the status of the pin // //***************************************************************************** extern uint8_t GPIO_getInputPinValue(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function enables the port interrupt on the selected pin //! //! This function enables the port interrupt on the selected pin. Note that //! only Port 1,2, A have this capability. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_PA //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxIE register. //! //! \return None // //***************************************************************************** extern void GPIO_enableInterrupt(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function disables the port interrupt on the selected pin //! //! This function disables the port interrupt on the selected pin. Note that //! only Port 1,2, A have this capability. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_PA //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxIE register. //! //! \return None // //***************************************************************************** extern void GPIO_disableInterrupt(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function gets the interrupt status of the selected pin //! //! This function gets the interrupt status of the selected pin. Note that only //! Port 1,2, A have this capability. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_PA //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! \return Logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! \n indicating the interrupt status of the selected pins [Default: //! 0] // //***************************************************************************** extern uint_fast16_t GPIO_getInterruptStatus(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function clears the interrupt flag on the selected pin //! //! This function clears the interrupt flag on the selected pin. Note that only //! Port 1,2,A have this capability. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_PA //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! //! Modified bits of \b PxIFG register. //! //! \return None // //***************************************************************************** extern void GPIO_clearInterruptFlag(uint_fast8_t selectedPort, uint_fast16_t selectedPins); //***************************************************************************** // //! \brief This function selects on what edge the port interrupt flag should be //! set for a transition //! //! This function selects on what edge the port interrupt flag should be set //! for a transition. Values for edgeSelect should be //! GPIO_LOW_TO_HIGH_TRANSITION or GPIO_HIGH_TO_LOW_TRANSITION. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Mask value is the logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15 //! \param edgeSelect specifies what transition sets the interrupt flag //! Valid values are: //! - \b GPIO_HIGH_TO_LOW_TRANSITION //! - \b GPIO_LOW_TO_HIGH_TRANSITION //! //! Modified bits of \b PxIES register. //! //! \return None // //***************************************************************************** extern void GPIO_interruptEdgeSelect(uint_fast8_t selectedPort, uint_fast16_t selectedPins, uint_fast8_t edgeSelect); //***************************************************************************** // //! \brief This function gets the interrupt status of the provided PIN and //! masks it with the interrupts that are actually enabled. This is //! useful for inside ISRs where the status of only the enabled //! interrupts needs to be checked. //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1 //! - \b GPIO_PORT_P2 //! - \b GPIO_PORT_P3 //! - \b GPIO_PORT_P4 //! - \b GPIO_PORT_P5 //! - \b GPIO_PORT_P6 //! - \b GPIO_PORT_P7 //! - \b GPIO_PORT_P8 //! - \b GPIO_PORT_P9 //! - \b GPIO_PORT_P10 //! - \b GPIO_PORT_P11 //! - \b GPIO_PORT_PJ //! //! \return Logical OR of any of the following: //! - \b GPIO_PIN0 //! - \b GPIO_PIN1 //! - \b GPIO_PIN2 //! - \b GPIO_PIN3 //! - \b GPIO_PIN4 //! - \b GPIO_PIN5 //! - \b GPIO_PIN6 //! - \b GPIO_PIN7 //! - \b GPIO_PIN8 //! - \b GPIO_PIN9 //! - \b GPIO_PIN10 //! - \b GPIO_PIN11 //! - \b GPIO_PIN12 //! - \b GPIO_PIN13 //! - \b GPIO_PIN14 //! - \b GPIO_PIN15, //! - \b PIN_ALL8, //! - \b PIN_ALL16 //! \n indicating the interrupt status of the selected pins [Default: //! 0] // //***************************************************************************** extern uint_fast16_t GPIO_getEnabledInterruptStatus(uint_fast8_t selectedPort); //***************************************************************************** // //! Registers an interrupt handler for the port interrupt. //! //! \param selectedPort is the port to register the interrupt handler //! //! \param intHandler is a pointer to the function to be called when the port //! interrupt occurs. //! //! This function registers the handler to be called when a port //! interrupt occurs. This function enables the global interrupt in the //! interrupt controller; specific GPIO interrupts must be enabled //! via GPIO_enableInterrupt(). It is the interrupt handler's responsibility to //! clear the interrupt source via GPIO_clearInterruptFlag(). //! //! Clock System can generate interrupts when //! //! \sa Interrupt_registerInterrupt() for important information about //! registering interrupt handlers. //! //! \return None. // //***************************************************************************** extern void GPIO_registerInterrupt(uint_fast8_t selectedPort, void (*intHandler)(void)); //***************************************************************************** // //! Unregisters the interrupt handler for the port. //! //! \param selectedPort is the port to unregister the interrupt handler //! //! This function unregisters the handler to be called when a port //! interrupt occurs. This function also masks off the interrupt in the //! interrupt controller so that the interrupt handler no longer is called. //! //! \sa Interrupt_registerInterrupt() for important information about //! registering interrupt handlers. //! //! \return None. // //***************************************************************************** extern void GPIO_unregisterInterrupt(uint_fast8_t selectedPort); //***************************************************************************** // //! This function sets the drive strength to high for the selected port //! //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1, //! - \b GPIO_PORT_P2, //! - \b GPIO_PORT_P3, //! - \b GPIO_PORT_P4, //! - \b GPIO_PORT_P5, //! - \b GPIO_PORT_P6, //! - \b GPIO_PORT_P7, //! - \b GPIO_PORT_P8, //! - \b GPIO_PORT_P9, //! - \b GPIO_PORT_P10, //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Valid values are: //! - \b GPIO_PIN0, //! - \b GPIO_PIN1, //! - \b GPIO_PIN2, //! - \b GPIO_PIN3, //! - \b GPIO_PIN4, //! - \b GPIO_PIN5, //! - \b GPIO_PIN6, //! - \b GPIO_PIN7, //! - \b GPIO_PIN8, //! - \b PIN_ALL8, //! //! \return None // //***************************************************************************** extern void GPIO_setDriveStrengthHigh(uint_fast8_t selectedPort, uint_fast8_t selectedPins); //***************************************************************************** // //! This function sets the drive strength to low for the selected port //! //! //! \param selectedPort is the selected port. //! Valid values are: //! - \b GPIO_PORT_P1, //! - \b GPIO_PORT_P2, //! - \b GPIO_PORT_P3, //! - \b GPIO_PORT_P4, //! - \b GPIO_PORT_P5, //! - \b GPIO_PORT_P6, //! - \b GPIO_PORT_P7, //! - \b GPIO_PORT_P8, //! - \b GPIO_PORT_P9, //! - \b GPIO_PORT_P10, //! - \b GPIO_PORT_PJ //! \param selectedPins is the specified pin in the selected port. //! Valid values are: //! - \b GPIO_PIN0, //! - \b GPIO_PIN1, //! - \b GPIO_PIN2, //! - \b GPIO_PIN3, //! - \b GPIO_PIN4, //! - \b GPIO_PIN5, //! - \b GPIO_PIN6, //! - \b GPIO_PIN7, //! - \b GPIO_PIN8, //! - \b PIN_ALL8, //! //! \return None // //***************************************************************************** extern void GPIO_setDriveStrengthLow(uint_fast8_t selectedPort, uint_fast8_t selectedPins); /* Backwards Compatibility Layer */ #define GPIO_selectInterruptEdge GPIO_interruptEdgeSelect #define GPIO_clearInterrupt GPIO_clearInterruptFlag //***************************************************************************** // // Mark the end of the C bindings section for C++ compilers. // //***************************************************************************** #ifdef __cplusplus } #endif //***************************************************************************** // // Close the Doxygen group. //! @} // //***************************************************************************** #endif // __GPIO_H__