This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP432P4011处理器 在不同运行模式下管脚处理

请问TI工程师:

       有一个问题咨询一下,我使用的是MSP432P4011处理器

       对于一些功能管脚,我在全速模式AM-48MHz下 是 使用的状态。

       因为大部分时间是 低功耗LF-128K模式运行,这些功能管脚是不使用的 状态。

       为了降低低功耗模式下的功耗,在低功耗运行状态时  这些管脚如何处理  是 变为普通模式 设置输出或者输入状态   还是保留全速模式 下的 功能态

  • 您现在是想使用低频率 low frequency 运行还是只是单纯地使用低功耗模式?

    能否详细说明下您现在需要的功能引脚?

    关于MSP432的 low frequency模式,我们有一个专门的文档,您可以看一下

    www.ti.com/.../slaa657b.pdf

    All peripherals are fully functional in the low-frequency power modes. The maximum operating frequency of the CPU, DMA, and all peripherals is limited to 128 kHz. External reset, all external interrupts, and wake-up sources are available in the low-frequency power modes. Peripheral interrupts can be raised and serviced as in the regular active modes.
  • 你好,Susan Yang
    我使用的系统模式如下
    正常运行时,运行在LPM0模式,然后如果没有用户操作,会转入LPM0_LF低频模式
    在这个LPM0_LF低频模式 下 很多在LPM0模式 下的功能脚 我对外连接着电路 ,但是此模式不用~~ 所以存在 是否需要优化处理的问题
  • All peripherals are fully functional in the low-frequency power modes. The maximum operating frequency of the CPU, DMA, and all peripherals is limited to 128 kHz. External reset, all external interrupts, and wake-up sources are available in the low-frequency power modes. Peripheral interrupts can be raised and serviced as in the regular active modes.

    按照我的理解是不需要额外做操作的。我会在确认后给您回复