1294开发板中ADC测量AIN2的电压,应怎么设置函数?急求解答,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您可以参考tivaware内的相关代码
C:\ti\TivaWare_C_Series-2.1.4.178\examples\peripherals\adc
//***************************************************************************** // // single_ended.c - Example demonstrating how to configure the ADC for // single ended operation. // // Copyright (c) 2010-2017 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // // This is part of revision 2.1.4.178 of the Tiva Firmware Development Package. // //***************************************************************************** #include <stdbool.h> #include <stdint.h> #include "inc/hw_memmap.h" #include "driverlib/adc.h" #include "driverlib/gpio.h" #include "driverlib/pin_map.h" #include "driverlib/sysctl.h" #include "driverlib/uart.h" #include "utils/uartstdio.h" //***************************************************************************** // //! \addtogroup adc_examples_list //! <h1>Single Ended ADC (single_ended)</h1> //! //! This example shows how to setup ADC0 as a single ended input and take a //! single sample on AIN0/PE3. //! //! This example uses the following peripherals and I/O signals. You must //! review these and change as needed for your own board: //! - ADC0 peripheral //! - GPIO Port E peripheral (for AIN0 pin) //! - AIN0 - PE3 //! //! The following UART signals are configured only for displaying console //! messages for this example. These are not required for operation of the //! ADC. //! - UART0 peripheral //! - GPIO Port A peripheral (for UART0 pins) //! - UART0RX - PA0 //! - UART0TX - PA1 //! //! This example uses the following interrupt handlers. To use this example //! in your own application you must add these interrupt handlers to your //! vector table. //! - None. // //***************************************************************************** //***************************************************************************** // // This function sets up UART0 to be used for a console to display information // as the example is running. // //***************************************************************************** void InitConsole(void) { // // Enable GPIO port A which is used for UART0 pins. // TODO: change this to whichever GPIO port you are using. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); // // Configure the pin muxing for UART0 functions on port A0 and A1. // This step is not necessary if your part does not support pin muxing. // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); // // Enable UART0 so that we can configure the clock. // SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); // // Use the internal 16MHz oscillator as the UART clock source. // UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC); // // Select the alternate (UART) function for these pins. // TODO: change this to select the port/pin you are using. // GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); // // Initialize the UART for console I/O. // UARTStdioConfig(0, 115200, 16000000); } //***************************************************************************** // // Configure ADC0 for a single-ended input and a single sample. Once the // sample is ready, an interrupt flag will be set. Using a polling method, // the data will be read then displayed on the console via UART0. // //***************************************************************************** int main(void) { #if defined(TARGET_IS_TM4C129_RA0) || \ defined(TARGET_IS_TM4C129_RA1) || \ defined(TARGET_IS_TM4C129_RA2) uint32_t ui32SysClock; #endif // // This array is used for storing the data read from the ADC FIFO. It // must be as large as the FIFO for the sequencer in use. This example // uses sequence 3 which has a FIFO depth of 1. If another sequence // was used with a deeper FIFO, then the array size must be changed. // uint32_t pui32ADC0Value[1]; // // Set the clocking to run at 20 MHz (200 MHz / 10) using the PLL. When // using the ADC, you must either use the PLL or supply a 16 MHz clock // source. // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the // crystal on your board. // #if defined(TARGET_IS_TM4C129_RA0) || \ defined(TARGET_IS_TM4C129_RA1) || \ defined(TARGET_IS_TM4C129_RA2) ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 20000000); #else SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); #endif // // Set up the serial console to use for displaying messages. This is // just for this example program and is not needed for ADC operation. // InitConsole(); // // Display the setup on the console. // UARTprintf("ADC ->\n"); UARTprintf(" Type: Single Ended\n"); UARTprintf(" Samples: One\n"); UARTprintf(" Update Rate: 250ms\n"); UARTprintf(" Input Pin: AIN0/PE3\n\n"); // // The ADC0 peripheral must be enabled for use. // SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); // // For this example ADC0 is used with AIN0 on port E7. // The actual port and pins used may be different on your part, consult // the data sheet for more information. GPIO port E needs to be enabled // so these pins can be used. // TODO: change this to whichever GPIO port you are using. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); // // Select the analog ADC function for these pins. // Consult the data sheet to see which functions are allocated per pin. // TODO: change this to select the port/pin you are using. // GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3); // // Enable sample sequence 3 with a processor signal trigger. Sequence 3 // will do a single sample when the processor sends a signal to start the // conversion. Each ADC module has 4 programmable sequences, sequence 0 // to sequence 3. This example is arbitrarily using sequence 3. // ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0); // // Configure step 0 on sequence 3. Sample channel 0 (ADC_CTL_CH0) in // single-ended mode (default) and configure the interrupt flag // (ADC_CTL_IE) to be set when the sample is done. Tell the ADC logic // that this is the last conversion on sequence 3 (ADC_CTL_END). Sequence // 3 has only one programmable step. Sequence 1 and 2 have 4 steps, and // sequence 0 has 8 programmable steps. Since we are only doing a single // conversion using sequence 3 we will only configure step 0. For more // information on the ADC sequences and steps, reference the datasheet. // ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_CH0 | ADC_CTL_IE | ADC_CTL_END); // // Since sample sequence 3 is now configured, it must be enabled. // ADCSequenceEnable(ADC0_BASE, 3); // // Clear the interrupt status flag. This is done to make sure the // interrupt flag is cleared before we sample. // ADCIntClear(ADC0_BASE, 3); // // Sample AIN0 forever. Display the value on the console. // while(1) { // // Trigger the ADC conversion. // ADCProcessorTrigger(ADC0_BASE, 3); // // Wait for conversion to be completed. // while(!ADCIntStatus(ADC0_BASE, 3, false)) { } // // Clear the ADC interrupt flag. // ADCIntClear(ADC0_BASE, 3); // // Read ADC Value. // ADCSequenceDataGet(ADC0_BASE, 3, pui32ADC0Value); // // Display the AIN0 (PE3) digital value on the console. // UARTprintf("AIN0 = %4d\r", pui32ADC0Value[0]); // // This function provides a means of generating a constant length // delay. The function delay (in cycles) = 3 * parameter. Delay // 250ms arbitrarily. // #if defined(TARGET_IS_TM4C129_RA0) || \ defined(TARGET_IS_TM4C129_RA1) || \ defined(TARGET_IS_TM4C129_RA2) SysCtlDelay(ui32SysClock / 12); #else SysCtlDelay(SysCtlClockGet() / 12); #endif } }