This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC26XX烧写projectzero后复位按键无效

如题。

CC26XX开发板,芯片是CC2652,烧写projectzero例程后发现按下reset按键没有用,设备不会复位。

过程描述:按下reset之前与BTool之间连好的,但是按下reset后连接断掉了且再scan也搜不到projectzero设备了,且串口没有日志输出,只能重新烧写程序。

同一块板子烧过simpleperipheral是正常的,按下reset按键后串口有输出菜单选项。

求大神指导。

  • 你也要把bim燒錄進去你的CC2652才行
  • 按照你说的重试了一遍,真的解决了!有几个问题想确认下:
    1.bim是每次烧写都要先烧进去才行吗?还是说只要烧一次就好了?(我之前有烧过的)
    2.bim是什么作用呢,我之前不按复位键没有用,但是蓝牙的连接和一些状态读取都是正常的,无线功能与bim没有关系吗?
    再次感谢你的回答!
  • 1. 如果沒有抹除晶片BIM 只要烧一次就好
    2. bim是Boot Image manager主要作用是OAD的時候來管理fw update用的,因為這個版本的ProjectZero有支持OAD所以必須要燒錄BIM,不然程序沒辦法跳轉到正確的位置
  • 我按照你说的试了一下,确实是只要烧一次就好,后面就算projectzero的程序有改动也没有关系。我之前应该是从simpleperipheral改烧projectzero的时候忘记重新烧一遍bim了,再次感谢大神!
  • This project is configured to be managed and launched by the BIM or Boot Image Manager example app. This means that this project does not include a CCFG section to configure the device at boot, and therefore requires that the BIM project is programmed into the device first.

    If BIM is not present in the device internal Flash, the project can usually be started from the IDE but will not be executed after a pin reset. Read more about BIM and OAD in the BLE5-Stack User’s Guide.

    具体信息您可以参考 下面链接给出的说明,希望对您有所帮助!

    dev.ti.com/.../