SDK版本为simplelink_cc13x2_26x2_sdk_4_10_00_78,使用官方例程simple_peripheral,通过CCS10.0版本编译下载后,点击运行,能够正常运行程序(可通过手机连接上广播),断电后重新上电,程序无法正常运行,无法再收到广播。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
YiKai Chen 说:如果你用的是有OAD功能的simple_peripheral例程、必須也要下載BIM到芯片
好像是不带OAD功能的,没有用例程名字带oad的那两个。
把編譯出來的軟件透過uiflash或者flash programmer 2下载後能運行嗎?
你的板子是TI的launchpad还是自己制作的,PRSC错误可能是硬件的问题,检查下晶振部分
公司自己设计的板子,我换了一个下载器后使用uniflash不会报PRSC错误了,也显示下载成功,问题依旧存在,下面为Uniflash下载的报告:
2020/7/8 下午2:06:40] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete.
[2020/7/8 下午2:06:42] [INFO] Cortex_M4_0: GEL Output: Memory Map Initialization Complete.
[2020/7/8 下午2:06:47] [INFO] Cortex_M4_0: GEL Output: Board Reset Complete.
[2020/7/8 下午2:06:59] [SUCCESS] Program Load completed successfully.