This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教 Sensor Controller CC2650 的代码

我想持续记录analog input 的值,每次记录相隔8ms,然后加上时间,透过蓝牙传出去。但

1.我不知道怎么加上时间

2.在另外一个电池电压管理的例子中,如果我想alarm在电压低于2.5的时候提醒我,应该怎么改

3.如果用蓝牙的话,是不是要有TASK-UART Emulator

我写了以下的代码:

持续记录

//Create variable int
U16 int;
//Enable the input of INT
gpioEnableInputBuf(AUXIO_I_INT);
//Input the INT's value into int
gpioGetInputValue(AUXIO_I_INT; int);

if (int == 1){
    //Set DSET to be high
    gpioSetOutput(AUXIO_XD_DSET);
    
    // Select ADC input
    adcSelectGpioInput(AUXIO_A_DOUT);
    
    // Enable the ADC;reference voltage is 4.7V and the sampling time is 2.7us; Timer trigger
    adcEnableSync(ADC_REF_FIXED, ADC_SAMPLE_TIME_2P7_US, ADC_TRIGGER_AUX_TIMER0);
    
    // Start ADC trigger timer at 12.5Hz (8ms)
    timer0Start(TIMER0_MODE_PERIODICAL, 24000,3);
    
    // Loop until the application sets the exit flag
    while (state.exit == 0) {
        
        // Wait for the next ADC sample and store it
        U16 n = state.head;
        adcReadFifo(output.pSamples[n]);
        
        // Update the head index
        utilIncrAndWrap(n, BUFFER_SIZE; state.head);
        
        // If ALERT interrupt generation is enabled
        if (state.alertEnabled == 1){
            
            // Calculate the number of samples currently stored
            S16 count = state.head - state.tail;
            if (count < 0) {
                count += BUFFER_SIZE;
            }
            
            // If above the configured threshold ...
            if (count >= cfg.alertThr){
                
                // Generate ALERT interrupt
                fwGenQuickAlertInterrupt();
                
                // Disable further generation to avoid unnecessary interrupts. It will be reenabled
                // by the application after handling the ALERT interrupt.
                state.alertEnabled = 0;
            }
            if (int==0){
                //clear the output on Dset
                gpioClearOutput(AUXIO_XD_DSET);
                // Generate ALERT interrupt
                fwGenQuickAlertInterrupt();
                
                // Disable further generation to avoid unnecessary interrupts. It will be reenabled
                // by the application after handling the ALERT interrupt.
                state.alertEnabled = 0;
            }
        }
    }
    
    // Stop the ADC trigger and flush the ADC FIFO
    timer0Stop();
    adcFlushFifo();
    
    // Disable the ADC
    adcDisable();
}

电池电压

// Select VDDS as input

adcSelectIntInput(ADC_INPUT_VDDS);


// Enable the ADC

adcEnableSync(ADC_REF_FIXED, ADC_SAMPLE_TIME_2P7_US, ADC_TRIGGER_MANUAL);


// Measure and store the result

adcGenManualTrigger();

U16 adcValue;

adcReadFifo(adcValue);

output.adcValue = adcValue;


// Disable the ADC

adcDisable();


// Check whether to notify the application (every time when below, once when returning above)

if (cfg.alarmEnable == 1) {



if (adcValue < cfg.alarmThr) {


output.alarm = 1;

fwGenAlertInterrupt();

} else {

if (output.alarm == 1) {

output.alarm = 0;

fwGenAlertInterrupt();

}

}

}


// Schedule the next execution

fwScheduleTask(5);