If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
[Su007]: Unable to open the command file "C:\ti\simplelink_cc2640r2_sdk_2_30_00_28\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_peripheral\tirtos\iar\app\..\config\configPkg\compiler.opt.defs" C:\Users\ADMINI~1\AppData\Local\Temp\EW6AAE.tmp 1
Error while running C/C++ Compiler
看你的图上用的是5X5,你自己的板子是什么?
这是需要的环境以及编译器:
IAR Embedded Workbench: EWARM-8.20.2
TI Code Composer Studio: CCS-8.2.0.0
TI Code Generation Tools for ARM: 18.01.03.LTS
XDCTools: 3.50.08.24
Cortex_M3_0: Can't Run Target CPU: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.188.0)
Cortex_M3_0: JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.188.0)