This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2f 内部DCDC供电模式 失效

Other Parts Discussed in Thread: CC2640R2F

我们焊接了3块CC2640R2f 测试板,选用DCDC供电模式,

第1只,开始一段时间内(数天),工作正常,后在将仿真器XDS110的USB端连接至一外部充电器,只取5V供电,XDS110配置成3.3V输出给测试板。之后发现DCDC_SW端没有输出,VDDR电压为零。断电测试DCDC_SW端的对地阻抗在100欧左右。

第2只,在带电状态下拔插测试板的供电USB接口,不是通过XDS110,也是拔插很多次后,发现DCDC_SW端没有输出,VDDR电压为零。断电测试DCDC_SW端的对地阻抗在20K左右。

第3只,目前工作正常。断电测试DCDC_SW端的对地阻抗在10M以上。

后将DCDC_SW输出不正常的2块测试板的DCDC 10UH电感拆掉,将供电模式改为LDO,CC2640R2f蓝牙及其他外设工作正常,VDDR电压达到1.67V。

在测试最开始时,10UH电感曾经焊接成1uH,VDDR输出也能达到1.67V,波形上会有毛刺,但24M晶体不能启振。

想咨询下,CC2640R2f的DCDC模块,在使用上有什么要特别注意的地方。

TI咨询.pdf