This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 CC2640 OAD功能

Other Parts Discussed in Thread: CC2540, CC2640, CC2640R2F

HI TI Team:

CC2540 和CC2640 OAD 功能,和设备扫描问题还请帮忙确认。

1.cc2540的large image OAD,相关源码下载: http://processors.wiki.ti.com/images/7/7e/Large_OAD_Example.zip

遇到的问题:如果用BLE Device Monitor+USB dongle升级,升级完成后,在BIM检查crc没办法通过,重新执行旧的image。官方推荐的multitool app已经下架了(APP升级软件),这个APK 是否还可以提供;

2.cc2640r2f multirole的OAD功能,自行移植总是失败,有文档可以参考的嘛?

3.确认cc2640r2f作为主机时,每个扫描周期,最多可以扫描多少个从机设备 (条件:从机的广播间隔比主机的扫描窗口快一倍)

以上为你还请帮忙,十分感谢!

谢谢!
吕春秋

  • 1、这个软件已经不再提供了
    2、文档请参考右边链接里的Add On-Chip OAD to an Existing Project:dev.ti.com/.../oad.html
    3、#define GAPCENTRALROLE_MAX_SCAN_RES 0x404

    Maximmum number of scan reports to store from GAPCentralRole_StartDiscovery (Read/Write)

    size: uint8_t

    default: 8

    range: 0-256 but this will be constrained by available RAM