This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于多角色例程相关问题

Other Parts Discussed in Thread: CC2640R2F

技术你好问几个问题:

一,我想咨询一下,是使用CC2640R2F芯片还有cc2640f128,这两个可以交错多主机连接同一个从机吗?(如一个cc2640r2f和一个cc2640r2f与cc2640f128)互相之间兼容吗?方法之类的有吗?

二,还有可以实现多个从机同时发送信息到主机吗?主机同时接收多个从机消息,这个主机是不是由于cc26系列芯片是单核的,同时接收这个是不可能对吧?一个时间只能做一件事。

三,我使用simplelink_cc2640r2_sdk_1_40_00_45这个协议栈,中的多角色例程,什么也不更改的话,给一个芯片烧写这个例程,是否这个芯片就是默认可以最多链接4个从机,我看宏定义(MAX_NUM_BLE_CONNS == 4)static uint8_t maxNumBleConns = MAX_NUM_BLE_CONNS;对吧?

DEFAULT_MAX_SCAN_RES这个宏定义我看描述,是说的可以最大搜索到15个正在广播的设备吗?

四,请问是否只有从机才可以广播。主机属性只是搜索广播的能力对吧?

希望依次回答谢谢